cancel
Showing results for 
Search instead for 
Did you mean: 

previously working UART interrupt not working when FreeRTOS preemptive task scheduling enabled

DBurr
Senior

Hi, I have some working code for STM32F746ZG that has a UART command line interface and FreeRTOS. It uses the "HAL_UART_Receive_IT" function and then waits for "HAL_UART_RxCpltCallback" function to set an OS flag when a character is received. When I have FreeRTOS preemptive task scheduling disabled everything works fine and dandy but when I enable preemptive task scheduling, the "HAL_UART_RxCpltCallback" doesn't fire. Any idea what I need to change for this to work with preemptive task scheduling?

If I change the thread priority of the UART thread to "Above Normal" then it works. It looks like when the priority is left at "Normal" the threads fails to start. Creating the thread appears to work but it never enters the thread function.

Thanks,

Doug

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0