cancel
Showing results for 
Search instead for 
Did you mean: 

OV5642 camera usage with STM32F7508-DK board

Sule_Akcay
Associate III

I want to use the OV5642 camera with the STM32F7508-DK card and display the image I take from the camera on the LCD screen on the card.

WhatsApp Görsel 2024-03-19 saat 10.07.54_dbf6842d.jpgWhatsApp Görsel 2024-03-19 saat 10.28.24_d99aa8e0.jpg

WhatsApp Görsel 2024-03-19 saat 10.07.54_d9e655b0.jpgWhatsApp Görsel 2024-03-19 saat 10.07.54_4fd2525c.jpg

Is this possible? If it is possible, can you help me how to do this?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
KDJEM.1
ST Employee

Hi @Sule_Akcay ,

I advise you to start your project using STM32CubeMx tool and STM32F7508-DK board  to configure DCMI GPIOs,  DCMI control signals, system clock......., then generate code and add drivers ov5642.c and ov5642.h.

After that , it is necessary to modify the main.c and main.h files by adding the adequate functions in the adequate spaces.

For that, you can refer to AN5020 and precisely 8.3 DCMI examples based on STM32CubeMX section and get inspired to create your own project.

I hope this help you!

Kaouthar

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

6 REPLIES 6
KDJEM.1
ST Employee

Hello @Sule_Akcay ,

It is mentioned in AN5020 "Introduction to digital camera interface (DCMI) for STM32 MCUs" that OV5642 as an ArduCAM 5 Megapixels camera module compatible with STM32 DCMI.

KDJEM1_0-1710834780317.png

For the connection between the camera module and STM32F7508-DK, I advise you to refer to the camera module datasheet and to board schematic. Note that this board has an "External Camera connector".

Also, I recommend you to start with an available example which is Camera. This example provides a short description of how to use the DCMI to interface with a camera module and to display in continuous or snapshot modes the picture on the LCD. This application has been tested with STM32F7508-DISCO board and OV9655 camera sensor and can be easily tailored to any other supported device and development board.

I hope this answer your request.

Thank you for your contribution in STCommunity :).

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Unfortunately, I do not have the OV9655 camera sensor.That's why I need to take images via SPI with the OV5642 camera module.

I would be glad if anyone can help with this issue.

Thanks :)

I found a sample application of the OV5642 camera module for the STM32F103C8T6 chip. However, I had difficulty adapting this code example to the STM32F7508-DK development board. Is there anyone who can help on this issue?

 

OV5642 camera module example application code for STM32F103C8T6 chip:

/**
  * @file    main.c
  * @author  Arducam 
  * @version V0.1
  * @date    2018.06.22
  * @brief   Minly work
  */

#include "main.h"

int main(void)
{
	uint8_t vid, pid, temp ;
	uint8_t Camera_WorkMode = 0;
	uint8_t start_shoot = 0;
	uint8_t stop = 0;
	NVIC_Configuration();
	SystemInit();
	delay_init();
	USART1_UART_Init(921600);
	ArduCAM_LED_init();
	ArduCAM_CS_init();
	sccb_bus_init();
	SPI1_Init();
	
	while(1)
	{
		write_reg(ARDUCHIP_TEST1, 0x55);
		temp = read_reg(ARDUCHIP_TEST1);
		if (temp != 0x55)
		{
			printf("ACK CMD SPI interface Error!\n");
			delay_ms(1000);
			continue;
		}
		else
		{
			printf("ACK CMD SPI interface OK!\r\n");
			break;
		}
	}
	
  while(1)
	{
		sensor_addr = 0x60;
		wrSensorReg8_8(0xff, 0x01);
		rdSensorReg8_8(OV2640_CHIPID_HIGH, &vid);
		rdSensorReg8_8(OV2640_CHIPID_LOW, &pid);
		if ((vid != 0x26 ) && (( pid != 0x41 ) || ( pid != 0x42 )))
			printf("ACK CMD Can't find OV2640 module!\r\n");
		else
		{
		  sensor_model =  OV2640 ;
		  printf("ACK CMD OV2640 detected.\r\n");   
		  break;
		}
		sensor_addr = 0x78;
		rdSensorReg16_8(OV5640_CHIPID_HIGH, &vid);
		rdSensorReg16_8(OV5640_CHIPID_LOW, &pid);
		if ((vid != 0x56) || (pid != 0x40))
			printf("ACK CMD Can't find OV5640 module!\r\n");
		else
		{
			sensor_model =  OV5640 ;
			printf("ACK CMD OV5640 detected.\r\n");
		  break;
		}
		sensor_addr = 0x78;
		rdSensorReg16_8(OV5642_CHIPID_HIGH, &vid);
		rdSensorReg16_8(OV5642_CHIPID_LOW, &pid);
		if ((vid != 0x56) || (pid != 0x42))
		{
			printf("ACK CMD Can't find OV5642 module!\r\n");
			continue;
		}
		else
		{
		 sensor_model =  OV5642 ;
		 printf("ACK CMD OV5642 detected.\r\n"); 
		 break;		 
		}
	}  
//Support OV2640/OV5640/OV5642 Init
  ArduCAM_Init(sensor_model);

	while(1)
	{
		if(NewCMD == 1)
		{
			NewCMD = 0;
			switch(USART1_RecieveData)
			{
				case 0:
					if (sensor_model == OV2640)
					{
						OV2640_set_JPEG_size(OV2640_160x120);
						printf("ACK CMD switch to OV2640_160x120\r\n");
					}
					else if(sensor_model == OV5640)
					{
						OV5640_set_JPEG_size(OV5640_320x240);
						printf("ACK CMD switch to OV5640_320x240\r\n");
					}
					else if(sensor_model == OV5642)
					{
						OV5642_set_JPEG_size(OV5642_320x240);
						printf("ACK CMD switch to OV5642_320x240\r\n");
					}
					break;
				case 1:
					if(sensor_model== OV2640)
					{
						OV2640_set_JPEG_size(OV2640_176x144);
						printf("ACK CMD switch to OV2640_176x144\r\n");
					}
					else if(sensor_model== OV5640)
					{ 
						OV5640_set_JPEG_size(OV5640_352x288);
						printf("ACK CMD switch to OV5640_352x288\r\n");
					}
					else if(sensor_model== OV5642)
					{ 
						OV5642_set_JPEG_size(OV5642_640x480);
						printf("ACK CMD switch to OV5642_640x480\r\n");
					}
					break;
				case 2:
					if(sensor_model== OV2640)
					{
						OV2640_set_JPEG_size(OV2640_320x240);
						printf("ACK CMD switch to OV2640_320x240\r\n");
					}
					else if(sensor_model== OV5640)
					{ 
						OV5640_set_JPEG_size(OV5640_640x480);
					printf("ACK CMD switch to OV5640_640x480\r\n");
					}
					else if(sensor_model== OV5642)
					{
						OV5642_set_JPEG_size(OV5642_1024x768);
						printf("ACK CMD switch to OV5642_1024x768\r\n");
					}
					break;
				case 3:
					if(sensor_model== OV2640)
					{
						OV2640_set_JPEG_size(OV2640_352x288);
						printf("ACK CMD switch to OV2640_352x288\r\n");
					}
					else if(sensor_model== OV5640)
					{ 
						OV5640_set_JPEG_size(OV5640_800x480);
						printf("ACK CMD switch to OV5640_800x480\r\n");
					}
					else if(sensor_model== OV5642)
					{
						OV5642_set_JPEG_size(OV5642_1280x960);
						printf("ACK CMD switch to OV5642_1280x960\r\n");
					}
					break;
				case 4:
					if(sensor_model== OV2640)
					{
						OV2640_set_JPEG_size(OV2640_640x480);
						printf("ACK CMD switch to OV2640_640x480\r\n");
					}
					else if(sensor_model== OV5640)
					{
						OV5640_set_JPEG_size(OV5640_1024x768);
						printf("ACK CMD switch to OV5640_1024x768\r\n");
					}
					else if(sensor_model== OV5642)
					{
						OV5642_set_JPEG_size(OV5642_1600x1200);	
						printf("ACK CMD switch to OV5642_1600x1200\r\n");
					}
					break;
				case 5:
					if(sensor_model== OV2640)
					{
						OV2640_set_JPEG_size(OV2640_800x600);
						printf("ACK CMD switch to OV2640_800x600\r\n");
					}
					else if(sensor_model== OV5640) 
					{
						OV5640_set_JPEG_size(OV5640_1280x960);
						printf("ACK CMD switch to OV5640_1280x960\r\n");
					}
					else if(sensor_model== OV5642)
					{
						OV5642_set_JPEG_size(OV5642_2048x1536);
						printf("ACK CMD switch to OV5642_2048x1536\r\n");
					}
					break;
				case 6:
					if(sensor_model== OV2640)
					{
						OV2640_set_JPEG_size(OV2640_1024x768);
						printf("ACK CMD switch to OV2640_1024x768\r\n");
					}
					else if(sensor_model== OV5640)
					{
						OV5640_set_JPEG_size(OV5640_1600x1200);
						printf("ACK CMD switch to OV5640_1600x1200\r\n");
					}
					else if(sensor_model== OV5642)
					{
						OV5642_set_JPEG_size(OV5642_2592x1944);	
						printf("ACK CMD switch to OV5642_2592x1944\r\n");
					}
					break;
				case 7:
					if(sensor_model== OV2640)
					{
						OV2640_set_JPEG_size(OV2640_1280x1024);
						printf("ACK CMD switch to OV2640_1280x1024\r\n");
					}
					else if(sensor_model== OV5640) 
					{
						OV5640_set_JPEG_size(OV5640_2048x1536);
						printf("ACK CMD switch to OV5640_2048x1536\r\n");
					}
					break;
				case 8:
					if(sensor_model== OV2640)
					{
						OV2640_set_JPEG_size(OV2640_1600x1200);
						printf("ACK CMD switch to OV2640_1600x1200\r\n");
					}
					else if(sensor_model== OV5640) 
					{
						OV5640_set_JPEG_size(OV5640_2592x1944);
						printf("ACK CMD switch to OV5640_2592x1944\r\n");
					}
					break;
				case 0x10:
					Camera_WorkMode = 1;
					start_shoot = 1;
					printf("ACK CMD CAM start single shoot.\r\n");
					break;
				case 0x11:
					set_format(JPEG);
					ArduCAM_Init(sensor_model);
					#if !defined(OV2640)
						set_bit(ARDUCHIP_TIM,VSYNC_MASK);
					#endif
					break;
				case 0x20:
					Camera_WorkMode = 2;
					start_shoot = 2;
					printf("ACK CMD CAM start video streaming.\r\n");
					break;
				case 0x21:
					stop = 1;
					printf("ACK CMD CAM stop video streaming.\r\n");
					break;
				case 0x30:
					Camera_WorkMode = 3;
					start_shoot = 3;
					printf("ACK CMD CAM start single shoot.\r\n");
					break;
				case 0x31:
					set_format(BMP);
					ArduCAM_Init(sensor_model);
					if(sensor_model != OV2640)
					{
						clear_bit(ARDUCHIP_TIM, VSYNC_LEVEL_MASK);
					}
					wrSensorReg16_8(0x3818,0x81);
					wrSensorReg16_8(0x3621,0xa7);		
					printf("ACK CMD SetToBMP \r\n");	
					break;
				default:
					break;
			}
		}
		if(Camera_WorkMode == 1)
		{
			if(start_shoot == 1)
			{
				start_shoot = 0;
				SingleCapTransfer();
			}
			if(receive_OK) 
			{
				receive_OK= 0;
				SendbyUSART1(); 
			}
		}	
		else if(Camera_WorkMode == 2)
		{
			if(start_shoot == 2)
			{
				if(send_OK)
				{
					if(stop)
					{
						printf("ACK CMD CAM stop video streaming.\r\n");
						stop = 0;
						Camera_WorkMode = 0;
						start_shoot = 0;
					}
					send_OK=false;    
					SingleCapTransfer();		
				}	
				if(receive_OK) 
				{
					receive_OK= 0;
					SendbyUSART1();   
				}
			}
		}
		else if(Camera_WorkMode == 3)
		{	
			if(start_shoot == 3)
			{
				start_shoot = 0;
				Camera_WorkMode = 0;
				StartBMPcapture();
			}
		}
	}
}

 

Program output:

WhatsApp Görsel 2024-03-25 saat 14.08.10_1e1b8492.jpg

Hi @Sule_Akcay ,

Can you detail the problem that you're encountering? 

Could you please check if you have communication between the MCU and the camera module?

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Of course.. I want to use the OV5642 camera with the STM32F7508-DK card and display the image I took from the camera on the LCD screen on the STM32F7508-DK card. But I don't know how to do this with software.

I found an example for the STM32F103 board, but I don't know how to adapt this example to the STM32F7508-DK board.

Can you help me with this?

 

KDJEM.1
ST Employee

Hi @Sule_Akcay ,

I advise you to start your project using STM32CubeMx tool and STM32F7508-DK board  to configure DCMI GPIOs,  DCMI control signals, system clock......., then generate code and add drivers ov5642.c and ov5642.h.

After that , it is necessary to modify the main.c and main.h files by adding the adequate functions in the adequate spaces.

For that, you can refer to AN5020 and precisely 8.3 DCMI examples based on STM32CubeMX section and get inspired to create your own project.

I hope this help you!

Kaouthar

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.