cancel
Showing results for 
Search instead for 
Did you mean: 

No source available for "<signal handler called>() at 0xfffffffe"

PranavBharadwaj
Associate

Hello,
I have been facing this issue of "No source available for "<signal handler called>() at 0xfffffffe"" on a nucleo-h753zi board. Following are few logs obtained from STMCube Programmer.
1. Fault that is eesca;ated to a hard fault (forced)
2. Faulty called function address: 0x1BB16608
3. Fault on instruction access (IACCVIOL)
4. MMFAR: 0x0
5. R0,R1,R2,R3,R12: 0x0
   SP:0xFFFFFFFC
   LR:0xFFFFFFFF
   PC:0xFFFFFFFE
   XPSR:0x1000003
6. Debugger issue: As soon as disassembly is clicked, debug is stopped. 

Note: I am trying to test CAN communication between two nucleo-h753zi boards. Code works on one of the boards. 

Any help would be much appretiated.

Thanks in advance

0 REPLIES 0