Need help for STM32F4 TCP/IP connection
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-05-07 11:55 PM
Posted on May 08, 2014 at 08:55
Hey,
I�m using the STM32F407ZG from the mikroe TFT starter kit. Now I want to get an Ethernet Connection with mikroemedia shield. The Connection should work over TCP/IP and DHCP can�t be used. I�m trying the example from the libstock site but I don�t get a physical Connection at least. I�m using the Net_Ethernet_Intern_STM32 libary from Libstock. When I try to initialize Ethernet then the linker hung up, if I comment it out then it works like before. Can anybody help me ? Thanks a lot #tcp/ip #stm32 #ethernet
Labels:
- Labels:
-
Ethernet
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-05-08 4:22 AM
Posted on May 08, 2014 at 13:22
When I try to initialize Ethernet then the linker hung up, if I comment it out then it works like before. Can anybody help me ?
I'm not using mikroemedia or libstock, so probably not much. If I decipher that properly, it hanging up in the reset/init code, probably stuck in a loop if you looked with a debugger. Most such problems relate to the clocking and PHY issues. Generating the correct clocks at 25/50 MHz, and configuring the correct pins for the mode used.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..