Mutliple TCP clients on STM32H563 with NetXDuo
I have a question regarding the tutorial "Handling multiple TCP clients on STM32H563 with NetX Duo" written by
In the first section "handling multilple clients on the same port", there is some example code. In the function
static VOID tcp_thread_entry(ULONG thread_input)
there is an infinite loop, containing a tx_queue_receive call:
/* Receive pointers to TCP socket and network packet from TCP callback */ ULONG msg[2]; status = tx_queue_receive(&g_tcp_q, msg, TX_WAIT_FOREVER);
At the moment I try to create an application based on this tutorial. Apparently, the tx_queue_receive fails (returns TX_QUEUE_ERROR) which makes sense, since no one sends data into the queue "g_tcp_q". At which point should this happen? I can't find it in the example code.
Furthermore, the tutorial states "You can find attached the file app_netxduo++clients_same_port.c that you can replace in this project to test this use case.". I can't find it.