cancel
Showing results for 
Search instead for 
Did you mean: 

LWIP SOCKET How can server tell if Client disconnected without "warning"? Server on MCU (STM32F429ZIT6, custom board), Client application on Windows I spent two days trying to figure a solution to this problem. Here is my solution, what do you think?

DPatr.2
Associate III
in main.c
int connectionClosed = 0;
...
Setup routine of socket
...
 while(1){
	  sin_size = sizeof(struct sockaddr_in);
	  new_socket = lwip_accept(s_create, (struct sockaddr *)&client_addr, &sin_size); 
	  if (new_socket > 0){
 
		  msgSize = sprintf(printMsg, "New client connected from IP: %s, Port: %d\r\n", inet_ntoa(client_addr.sin_addr), ntohs(client_addr.sin_port));
		  HAL_UART_Transmit(&huart3, (uint8_t*)printMsg, msgSize, 10);
		  connectionClosed = 0;
 
		  while(strncmp(recvBuff,"close", 5)){
 
			 if (connectionClosed) {
				  goto socket_close;
			 }
 
			  memset(recvBuff, 0, sizeof(recvBuff));
			  retVal = lwip_recv(new_socket, recvBuff, sizeof(recvBuff), MSG_DONTWAIT); 
			  // Process buffer
			  processMsg(recvBuff);
 
			  //Toggle LED every ~second
			  updateLED();
 
			  osDelay(1);
		  }// End of client connected loop
 
		  socket_close:
		  lwip_close(new_socket);
 
	  }
}
 
 
in sockets.c
extern connectionClosed;
 
static void
event_callback(struct netconn *conn, enum netconn_evt evt, u16_t len)
{
  int s, check_waiters;
  struct lwip_sock *sock;
  SYS_ARCH_DECL_PROTECT(lev);
 
  LWIP_UNUSED_ARG(len);
 
  /* Get socket */
  if (conn) {
    s = conn->socket;
    if (s < 0) {
      /* Data comes in right away after an accept, even though
       * the server task might not have created a new socket yet.
       * Just count down (or up) if that's the case and we
       * will use the data later. Note that only receive events
       * can happen before the new socket is set up. */
      SYS_ARCH_PROTECT(lev);
      if (conn->socket < 0) {
        if (evt == NETCONN_EVT_RCVPLUS) {
          /* conn->socket is -1 on initialization
             lwip_accept adjusts sock->recvevent if conn->socket < -1 */
          conn->socket--;
        }
        SYS_ARCH_UNPROTECT(lev);
        return;
      }
      s = conn->socket;
      SYS_ARCH_UNPROTECT(lev);
    }
 
    sock = get_socket(s);
    if (!sock) {
      return;
    }
  } else {
    return;
  }
 
  check_waiters = 1;
  SYS_ARCH_PROTECT(lev);
  /* Set event as required */
  switch (evt) {
    case NETCONN_EVT_RCVPLUS:
      sock->rcvevent++;
      if (sock->rcvevent > 1) {
        check_waiters = 0;
      }
      break;
    case NETCONN_EVT_RCVMINUS:
      sock->rcvevent--;
      check_waiters = 0;
      break;
    case NETCONN_EVT_SENDPLUS:
      if (sock->sendevent) {
        check_waiters = 0;
      }
      sock->sendevent = 1;
      break;
    case NETCONN_EVT_SENDMINUS:
      sock->sendevent = 0;
      check_waiters = 0;
      break;
    case NETCONN_EVT_ERROR:
      sock->errevent = 1;
      connectionClosed = 1;
      break;
    default:
      LWIP_ASSERT("unknown event", 0);
      break;
  }
 
  if (sock->select_waiting && check_waiters) {
    /* Save which events are active */
    int has_recvevent, has_sendevent, has_errevent;
    has_recvevent = sock->rcvevent > 0;
    has_sendevent = sock->sendevent != 0;
    has_errevent = sock->errevent != 0;
    SYS_ARCH_UNPROTECT(lev);
    /* Check any select calls waiting on this socket */
    select_check_waiters(s, has_recvevent, has_sendevent, has_errevent);
  } else {
    SYS_ARCH_UNPROTECT(lev);
  }
  done_socket(sock);
}
 

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0