cancel
Showing results for 
Search instead for 
Did you mean: 

Looks like a silIcon bug in MAC Ethernet controller on STM32H753 MCU: unexpected IRQ execution after transmittion of 0x80000000 packets

leshich-k
Associate II

Hi everybody. 

We're facing some issues with MAC Ethernet controller on STM32H753 MCU. Situation looks like a silicon bug: after transmitting of 2147483648 (0x80000000) packets over Ethernet the internal MAC controller in the specific circumstances starts generating the unexpected interrupts that cannot be handled in IRQ handler since there are no appropriate bits available in DMACSR register. As a result the normal MCU working is stopped by the infinite Ethernet interrupt execution. Only reinitialization of the MAC controller helps to recover a normal MCU working.

Has anyone faced the same behaviour during MAC Ethernet packets transmittion?

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
waclawek.jan
Super User

Yes, this is a very similar to our situation, except that we are using STM32H7 MCU. It looks strange that we didn't face it in our earlier projects that used STM32F7 MCUs.

waclawek.jan
Super User

There are differences in the details of implementation, see given thread and the RM. Also, if you use any "library" such as Cube, it might've been adressed there, in the 'F7 version.

JW

You're right! We were using MAC Ethernet driver EMAC_STM32F7xx from MRK-ARM library that already contained some code to disable the MMC interrupts.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.