2025-12-08 1:21 AM - last edited on 2025-12-08 1:35 AM by mƎALLEm
I’m currently working on an STM32 project with Ethernet connectivity and LwIP. I want to know the IP address of the STM32 while configuring the network settings in CubeIDE.
Here’s my setup:
STM32 is connected to a router via an Ethernet cable and my laptop is also connected to same router via wifi.
LwIP is being used as the TCP/IP stack.
In LwIP settings, there is an option to choose DHCP or Static IP.
My questions are:
If I enable DHCP, how can I find out the dynamically assigned IP of the STM32?
If I use a Static IP, what are the correct parameters to set (IP, Subnet Mask, Gateway) to ensure the STM32 is reachable from my PC?
Are there any tips or methods to quickly verify the STM32’s IP on the network, such as through serial print, ping, or a network scanner?