cancel
Showing results for 
Search instead for 
Did you mean: 

internal CAN bootloader in connectivity line devices

jurek
Associate
Posted on January 08, 2013 at 10:55

I would like to test the built in bootloader of the STM32F105VC using the CAN bus to make sure it (the bootloader) could be used in our product. I was wondering if anyone here could support me with a program, which could be used to flash the uC through CAN. I've got an ESD CAN-USB/2 but a program using an API different to ESD's would also be of great value - it would greatly shorten our prototyping process.

#connectivity-can-bootloader
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0