cancel
Showing results for 
Search instead for 
Did you mean: 

IAR debugger - Difference between specifying STM32H750B-DK and just STM32H750IB chip.

CChen.16
Associate II

We are using IAR embedded workbench for our compiler and debugger (I-jet). I am testing with a STM32H750B-DK board. Running the sample code of QSPI memory mapped. I realized that if I select board as STM32H750-DK, then everything works fine, but if I select STM32H750IB, then the flash reading was always 0x99. What is the difference between the two selections? Does the debugger load extra initialization code for DK board? The source code is exactly the same. 

Thanks for any help in advance.

2 REPLIES 2
Andrew Neil
Super User

@CChen.16 wrote:

We are using IAR embedded workbench for our compiler and debugger (I-jet) ... Does the debugger load extra initialization code for DK board? 


You really need to ask IAR about the specific behaviour of their product.

https://www.iar.com/support 

 

Anyhow, when you tell it the DK, then it will presumably have full details of the board and its memory configuration, etc.

If you just tell it the chip part number, it won't know anything but the chip - it will have no idea about any external connections. You will provide all that info - did you?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Pavel A.
Super User

IAR has "board definition" files (*.board)  where you specify the "external memory loaders" script  (*.flash) and executable drivers (*.out).  Please look at these files for the DK board to understand how to change them for your custom board.