cancel
Showing results for 
Search instead for 
Did you mean: 

I am planning to use Nucleo-STM32G071RB and Nucleo-USBPDM1 boards to develop a 100W battery charger. Is it possible to achieve upto 21 V with programmable power supply (PPS) regulation with this setup?

DRoy.3
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
MROUV.1
ST Employee

X-NUCLEO-SNK1M1 or X-NUCLEO-USBPDM1 are 22V compliant with on Vbus

Type-C Port Protection : TCPP01-M12 22V

TVS : ESDA25P35-1U1M 22V

N-MOSFET : STL11N3LLH6 30V

LDO : ST715PU33R 24V

View solution in original post

2 REPLIES 2
MROUV.1
ST Employee

Dear,

It's possible to reach 21V PPS with this setup.

The maximum DC voltage on Vbus is 22V.

MROUV.1
ST Employee

X-NUCLEO-SNK1M1 or X-NUCLEO-USBPDM1 are 22V compliant with on Vbus

Type-C Port Protection : TCPP01-M12 22V

TVS : ESDA25P35-1U1M 22V

N-MOSFET : STL11N3LLH6 30V

LDO : ST715PU33R 24V