cancel
Showing results for 
Search instead for 
Did you mean: 

HTTP to HTTPS web server on STM32H735G-DK based on examples

slime
Associate II

I am trying to implement an TLS HTTPS server based on this HTTP Web Server sample:

https://github.com/STMicroelectronics/x-cube-azrtos-h7/tree/main/Projects/STM32H735G-DK/Applications/NetXDuo/Nx_WebServer

I have been trying to convert the above sample to TLS HTTPS from this example code functions from the same GIT hub:

https://github.com/STMicroelectronics/x-cube-azrtos-h7/blob/main/Middlewares/ST/netxduo/samples/demo_netxduo_https.c

But I can't get the server to respond correctly from the clientHello, it responds with a short packet that should have been a serverHello. Using Wireshark to verify this.

The HTTP sample works fine on the STM32H735G-DK as it should. 

I have also tried adapting the process described in Small Example System (TLS Web Server):

https://docs.microsoft.com/en-us/azure/rtos/netx-duo/netx-secure-tls/chapter2

The example above uses different functions than the STM32 hosted examples, but still have the same broken server response. I am sort of stuck now. I am posting this here because it looks like STM employees ported the Azure middleware over from Microsoft.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
slime
Associate II

Adding a #define NX_SECURE_ENABLE_AEAD_CIPHER to nx_user.h fixed the issue and now has a total of 7 cipher suites available.

View solution in original post

2 REPLIES 2
slime
Associate II

The response packet isn't corrupted. The issue seems to be there are only 4 supported cipher suites on the STM32 NetXDuo HTTPS server, and all modern browsers like Chrome, Edge, & Firefox deny the use of those 4 available. They are:

0xC023 TLS_ECDHE_ECDSA_WITH_AES_128_CBC_SHA256

0xC027 TLS_ECDHE_RSA_WITH_AES_128_CBC_SHA256

0x003d  TLS_RSA_WITH_AES_256_CBC_SHA256

0x003c  TLS_RSA_WITH_AES_128_CBC_SHA256

Microsoft Internet Explorer does work. The remaining question is why only those 4 and is there a way to add newer cipher suites without trashing the NetXDuo platform?

slime
Associate II

Adding a #define NX_SECURE_ENABLE_AEAD_CIPHER to nx_user.h fixed the issue and now has a total of 7 cipher suites available.