2018-05-31 7:58 AM
Hi everyone,
I have a STM32F7 Discovery board and I would like to upload new firmware on it.
I read AN2606 and AN4826, and I saw that it's possible to split the flash into two memory banks (nDBank = 0) and I can start either on one or the other bank using BOOT_ADD0.
I have downloaded the extended_cube_dbank_f7 file that provide an example of dual bank boot. I followed every steps, which isn't hard, but I am still not able to boot on the second bank whether I change BOOT_ADD0.
I have used STM32 Utility to configure my MCU (unchecked nDBank in Option Bytes, while nDBoot is still checked), I have programmed the two banks with different firmware @0x08000000 and
@0x08100000.
The BOOT_ADD0 parameter, under Boot adress option bytes section, has no effect whether I use 0x0080 or 0x0081. I can boot @0x08000000 but it seems like something goes wrong when I try to start @0x08
1
00000!
I followed the tutorial step by step, did I miss something?
Thanks for the help.
Ced.
#stm32f7 #dual-bank-bootSolved! Go to Solution.
2018-06-01 5:00 AM
Uncheck nDBoot. BOOT_ADD0 needs to be 0x2000 to boot from Bank0 or 0x2040 to boot from Bank1.
2018-06-01 5:00 AM
Uncheck nDBoot. BOOT_ADD0 needs to be 0x2000 to boot from Bank0 or 0x2040 to boot from Bank1.
2018-06-04 3:11 AM
Hi Doug,
Thank you, you were right. I misunderstood the concept of nDBoot. I thought it was only useful to select BOOT_ADD0 or BOOT_ADD1 adresses through Boot0 pin.
Anyway, it works and I'm back on track.
Have a good day,
Ced.
2018-06-04 3:20 AM
Hi
cedric.seguin
,https://community.st.com/0D50X00009bMM5DSAW
-Nesrine-