cancel
Showing results for 
Search instead for 
Did you mean: 

How to resolve the error "libusb_open() failed with LIBUSB_ERROR_NOT_SUPPORTED" when connecting to openOCD from command line?

ABora.2
Associate

I am trying to debug my STM32 NUCLEO-F334R8 board. When I try to connect to the board via openocd from the command line . I get the following log:

openocd -f board/st_nucleo_f3.cfg

GNU MCU Eclipse 64-bits Open On-Chip Debugger 0.10.0+dev-00254-g2ec04e4e (2017-11-10-11:34)

Licensed under GNU GPL v2

adapter speed: 1000 kHz

adapter_nsrst_delay: 100

Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD

none separate

Info : Unable to match requested speed 1000 kHz, using 950 kHz

Info : Unable to match requested speed 1000 kHz, using 950 kHz

Info : clock speed 950 kHz

Error: libusb_open() failed with LIBUSB_ERROR_NOT_SUPPORTED

Info : STLINK v2 JTAG v39 API v2 SWIM v27 VID 0x0483 PID 0x374B

Info : using stlink api v2

Info : Target voltage: 3.255227

Info : stm32f3x.cpu: hardware has 6 breakpoints, 4 watchpoints

Info : Listening on port 3333 for gdb connections

srst_only separate srst_nogate srst_open_drain connect_deassert_srst

Info : Listening on port 6666 for tcl connections

Info : Listening on port 4444 for telnet connections

It gets connected to openOCD but how to resolve the error "libusb_open() failed with LIBUSB_ERROR_NOT_SUPPORTED"?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0