cancel
Showing results for 
Search instead for 
Did you mean: 

How to quckly test CAN module using SPL?

GKlim
Associate II

Hello! I'm working on project requaring CAN node. I decided to quckly check if the periphery is configured correcltly. For this purpose I connected two pull-ups resistors to Rx and Tx pins and tried to see some bits on the oscilloscope.

I configured GPIOs (as Alternate Function and Open Drain output), CAN and CAN's filters. Inside the "while(1)" cycle I tried to send some message. But there is no bits on th oscilloscope.

Here is my code.

I have 2 questions. Is it possible to test my software configuration the way I describe?

Could you review the code and explain what is wrong with that, please?

#include "stm32f0xx.h"
#include "stm32f0xx_rcc.h"
#include "stm32f0xx_gpio.h"
#include "stm32f0xx_can.h"
void CAN1_Init(void)
{
	RCC_APB1PeriphClockCmd(RCC_APB1Periph_CAN1,ENABLE);
 
	CAN_OperatingModeRequest(CAN1,CAN_OperatingMode_Initialization);
 
	CAN_InitTypeDef CAN;
	CAN.CAN_Prescaler=100;
	CAN.CAN_Mode=CAN_Mode_Normal;
	CAN.CAN_SJW=CAN_SJW_1tq;
	CAN.CAN_BS1=CAN_BS1_4tq;
	CAN.CAN_BS2=CAN_BS1_3tq;
	CAN.CAN_TTCM=DISABLE;
	CAN.CAN_ABOM=DISABLE;
	CAN.CAN_AWUM=DISABLE;
	CAN.CAN_NART=DISABLE;
	CAN.CAN_RFLM=DISABLE;
	CAN.CAN_TXFP=DISABLE;
	CAN_StructInit(&CAN);
 
	CAN_ITConfig(CAN1,CAN_IT_FF0,ENABLE);
}
void CAN1_Filter_Init(void)
{
	CAN_FilterInitTypeDef FILT;
	FILT.CAN_FilterNumber = 0;
	FILT.CAN_FilterMode = CAN_FilterMode_IdList;
	FILT.CAN_FilterScale = CAN_FilterScale_16bit;
	FILT.CAN_FilterIdHigh = 0x53A<<5;
	FILT.CAN_FilterIdLow = 0x53D<<5;
	FILT.CAN_FilterMaskIdHigh = 0x54D<<5;
	FILT.CAN_FilterMaskIdLow = 0x54F<<5;
	FILT.CAN_FilterFIFOAssignment = 0;
	FILT.CAN_FilterActivation = ENABLE;
	CAN_FilterInit(&FILT);
 
	FILT.CAN_FilterNumber = 1;
	FILT.CAN_FilterIdHigh = 0xA<<5;
	FILT.CAN_FilterIdLow = 0x33<<5;
	FILT.CAN_FilterMaskIdHigh = 0x44<<5;
	FILT.CAN_FilterMaskIdLow = 0x55<<5;
	CAN_FilterInit(&FILT);
}
void GPIOA_Init(void)
{
	GPIO_InitTypeDef GPIO_InitStructure;
	RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
	GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11|GPIO_Pin_12;
	GPIO_InitStructure.GPIO_OType = GPIO_OType_OD;
	GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
	GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
	GPIO_PinAFConfig(GPIOA,GPIO_PinSource11,GPIO_AF_4);
	GPIO_PinAFConfig(GPIOA,GPIO_PinSource12,GPIO_AF_4);
	GPIO_Init(GPIOA, &GPIO_InitStructure);
 
	NVIC_SetPriority(CEC_CAN_IRQn,1);
	NVIC_EnableIRQ(CEC_CAN_IRQn);
 
}
void CEC_CAN_IRQHandler()
{
	/*HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_3);
	CAN_ID = CanHandle->pRxMsg->StdId;
	CAN_DLC = CanHandle->pRxMsg->DLC;
	DATA[0] = CanHandle->pRxMsg->Data[0];
	DATA[1] = CanHandle->pRxMsg->Data[1];
	DATA[2] = CanHandle->pRxMsg->Data[2];
	DATA[3] = CanHandle->pRxMsg->Data[3];
	DATA[4] = CanHandle->pRxMsg->Data[4];
	DATA[5] = CanHandle->pRxMsg->Data[5];
	DATA[6] = CanHandle->pRxMsg->Data[6];
	DATA[7] = CanHandle->pRxMsg->Data[7];
	HAL_CAN_Receive_IT(&hcan, CAN_FIFO0);*/
	//CAN_Receive()
}
 
int main(void)
{
	RCC_APB1PeriphClockCmd(RCC_APB1Periph_CAN1, ENABLE);
	GPIOA_Init();
	CAN1_Init();
	CAN1_Filter_Init();
 
	CanTxMsg Message;
	Message.StdId=0x222;
	Message.DLC=1;
	Message.Data[0]=83;
	
	CAN_OperatingModeRequest(CAN1,CAN_OperatingMode_Normal);
	
    while(1)
    {
    	CAN_Transmit(CAN1,&Message);
    	int i = 0;
    	for (i = 0; i < 1000000; ++i) {}
    }
}

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
KnarfB
Super User

> I connected two pull-ups resistors to Rx and Tx

Try connecting RX and TX. On a regular bus, RX is also listening to its own messages sent by TX.