How to program a STM32 Nucleo board via Ethernet interface?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-05-08 3:25 AM
Hi,
is there a way to program a STM32 Nucleo board (Nucleo-F767ZI) via the Ethernet interface?
The problem with the usb port is when the Nucleo 5V is powered externally via the E5V pin, at power on of the 5V, the usb cable must be removed. So on a remote system someone has to connect the usb cable first before I can program the Nucleo. So if I can program the Nucleo via the Ethernet interface, I can avoid this problem.
Best regards,
Luc
Labels:
- Labels:
-
Ethernet
-
STM32F7 Series
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0