cancel
Showing results for 
Search instead for 
Did you mean: 

How can I start rtos programming for stm32f217xx controller.

Trinu
Associate III

Hi ,

I want configure the UART and GPIO peripherals using RTOS(RTx) .

here I am using keil5 u version .And STM32F217xx controller (custom board )

Already I was done configuration for gpio.

/*----------------------------------------------------------------------------
 
 * CMSIS-RTOS 'main' function template
 
 *---------------------------------------------------------------------------*/
 
 
 
#include "RTE_Components.h"
#include CMSIS_device_header
#include "cmsis_os2.h"
 
 
 
 void gpio_Initfun(void);
 
/*
 * led initialization.
 *
 */
 
 
 
 void gpio_Initfun(void)
 
 {
	 GPIOF->MODER |=0x00000005; 
	 GPIOF->OTYPER |=0x00000000;
	 GPIOF->OSPEEDR |=0x00000005;
	 GPIOF->PUPDR |=0x00000005;
	 GPIOF->ODR |=0x000000000;
 
 }
/*----------------------------------------------------------------------------
 
 * Application functions thread
 
 *---------------------------------------------------------------------------*/
 
__NO_RETURN static void ledTwo (void *argument) {
 
 (void)argument;
 while(1)
 
	{
		osDelay(500);
		GPIOF->ODR &= ~(unsigned int)(0x0000001); 
		osDelay(500);
		GPIOF->ODR |= 0x0000001;
	}
}
 
__NO_RETURN static void ledOne (void *argument) {
 (void)argument;
 while(1)
	{
		osDelay(500);
		GPIOF->ODR &= ~(unsigned int)(0x0000002);
		osDelay(500);
		GPIOF->ODR |= 0x0000002;
	}
 
}
 
 
 
 
 
int main (void) {
 
   SET_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOFEN); 
   SystemCoreClockUpdate(); 
    osKernelInitialize();       
    gpio_Initfun();
 
    osThreadNew(ledTwo, NULL, NULL);
    osThreadNew(ledOne, NULL, NULL);
 
 osKernelStart();           
 
  while(1);
 
}

the above code is working.

Instead of using the SFR programming I want to use predefined librariesf or programming the my controller.

Please some one guide me how to use STM32 predefined libraries in RTOS programming.

thanks in advance.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Bowman32
ST Employee

Hi,

You can refer to provided FreeRTOS examples within STM32CubeF2 firmware via this path: STM32Cube_FW_F2_V1.8.0\Projects\STM322xG_EVAL\Applications\FreeRTOS

Bouraoui

View solution in original post

1 REPLY 1
Bowman32
ST Employee

Hi,

You can refer to provided FreeRTOS examples within STM32CubeF2 firmware via this path: STM32Cube_FW_F2_V1.8.0\Projects\STM322xG_EVAL\Applications\FreeRTOS

Bouraoui