cancel
Showing results for 
Search instead for 
Did you mean: 

Hi ,i have created a file stm32.txt by porting fatfs into flash and verified write and read baremetal,now can this file be visible to my pc if i bring up and add an usb interface msc device config.Is this possible .

svii
Associate III

I have done this:

1) created a file using fatfs on flash open and read ,it is working.

2) created a usb interface configured as msc device,when plugged into pc, new drive gets created, however it asks to format it. I have added only

read functionality of flash to this:

STORAGE_Read_FS(uint8_t lun, uint8_t *buf, uint32_t blk_addr, uint16_t blk_len) . not added write functionality.

/////////////////////////////////////main.c//////////////////////////////////////////

USBD_Init(&hUsbDeviceFS, &FS_Desc, DEVICE_FS);

 USBD_RegisterClass(&hUsbDeviceFS, &USBD_MSC);

USBD_MSC_RegisterStorage(&hUsbDeviceFS,&USBD_Storage_Interface_fops_FS);  

USBD_Start(&hUsbDeviceFS); 

 if( FATFS_LinkDriver(&USER_Driver, USERPath)== 0)

{

  /*##-2- Init the SD Card #################################################*/

#if FATFS_MKFS_ALLOWED

   FRESULT res;

    res = f_mkfs(USERPath, FM_ANY, 0, workBuffer, 4096);

   if (res != FR_OK)

   {

    Error_Handler();

   }

#endif

 FS_FileOperations();

the usb does not detect the file stm32.txt created , fs_fileoperation also fails .

what is wrong ,thanks in advance.

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6

I wouldn't try to access them both concurrently, but yes a correctly built MSC device should be able to access a FatFs created volume on a PC.

The MSC would need to report the capacity and block size used.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Hi, i am not able to format the flash below is the code :

int8_t STORAGE_Read_FS(uint8_t lun, uint8_t *buf, uint32_t blk_addr, uint16_t blk_len)

{

  

uint32_t add_blk = 0;

add_blk = blk_addr;

uint32_t a0 = 0;

uint32_t a1 = 0;

  

a0 = add_blk * 512;   

 a1 = blk_len * 1;

 SST80B_ReadSector(buf,0,a0,a1);

  

 return (USBD_OK);

  

}

int8_t STORAGE_Write_FS(uint8_t lun, uint8_t *buf, uint32_t blk_addr, uint16_t blk_len)

{

uint8_t temp_b0[512] ={0};

 uint8_t temp_b1[512] ={0};

 uint8_t temp_b2[512] ={0};

 uint8_t temp_b3[512] ={0};

 uint8_t temp_b4[512] ={0};

 uint8_t temp_b5[512] ={0};

 uint8_t temp_b6[512] ={0};

 uint8_t temp_b7[512] ={0};

 uint32_t a0 = 0;

 uint32_t a1 = 0;

 a0 = add_blk * 512;   

 a1 = blk_len * 1;

 uint32_t add_data0 = (a0/4096); 

 uint32_t add_data1 = add_data0 * 4096; 

 uint32_t blka = a0;  

 uint32_t blkc = 0;

 SST80B_ReadSector(temp_b1,0,(add_data1+512),512);

 SST80B_ReadSector(temp_b2,0,(add_data1+1024),512);

 SST80B_ReadSector(temp_b3,0,(add_data1+1536),512);

 SST80B_ReadSector(temp_b4,0,(add_data1+2048),512);

 SST80B_ReadSector(temp_b5,0,(add_data1+2560),512);

 SST80B_ReadSector(temp_b6,0,(add_data1+3072),512);

 SST80B_ReadSector(temp_b7,0,(add_data1+3584),512);

 if(blka < 512)

 blkc = 1;

 else if ((blka >= 512)&& (blka < 1024))

 blkc = 2; 

 else if ((blka >= 1024)&& (blka < 1536))

 blkc = 3; 

 else if ((blka >= 1536)&& (blka < 2048))

 blkc = 4;

 else if ((blka >= 2048)&& (blka < 2560))

 blkc = 5;

 else if ((blka >= 2560)&& (blka < 3072))

 blkc = 6;

 else if ((blka >= 3072)&& (blka < 3584))

 blkc = 7;

 else

 blkc =8; 

 chipsector_erase_call(add_data1);

 if(blkc == 1)

 {

SST25Write((a0),(uint8_t *)buf,512);

SST25Write((add_data1+512),(uint8_t *)temp_b1,512);

SST25Write((add_data1+1024),(uint8_t *)temp_b2,512);

SST25Write((add_data1+1536),(uint8_t *)temp_b3,512);

SST25Write((add_data1+2048),(uint8_t *)temp_b4,512);

SST25Write((add_data1+2560),(uint8_t *)temp_b5,512);

SST25Write((add_data1+3072),(uint8_t *)temp_b6,512);

SST25Write((add_data1+3584),(uint8_t *)temp_b7,512);

blkc = 0;

 }

if(blkc == 2)

 {

SST25Write(a0,(uint8_t *)buf,512);

SST25Write((add_data1),(uint8_t *)temp_b0,512);

SST25Write((add_data1+1024),(uint8_t *)temp_b2,512);

SST25Write((add_data1+1536),(uint8_t *)temp_b3,512);

SST25Write((add_data1+2048),(uint8_t *)temp_b4,512);

SST25Write((add_data1+2560),(uint8_t *)temp_b5,512);

SST25Write((add_data1+3072),(uint8_t *)temp_b6,512);

SST25Write((add_data1+3584),(uint8_t *)temp_b7,512);

 blkc = 0;

 }

if(blkc == 3)

 {

SST25Write((a0),(uint8_t *)buf,512);

SST25Write((add_data1),(uint8_t *)temp_b0,512);

SST25Write((add_data1+512),(uint8_t *)temp_b1,512);

SST25Write((add_data1+1536),(uint8_t *)temp_b3,512);

SST25Write((add_data1+2048),(uint8_t *)temp_b4,512);

SST25Write((add_data1+2560),(uint8_t *)temp_b5,512);

SST25Write((add_data1+3072),(uint8_t *)temp_b6,512);

SST25Write((add_data1+3584),(uint8_t *)temp_b7,512);

blkc = 0;

 }

  

if(blkc == 4)

 {

SST25Write((a0),(uint8_t *)buf,512);

SST25Write((add_data1),(uint8_t *)temp_b0,512);

SST25Write((add_data1+512),(uint8_t *)temp_b1,512);

SST25Write((add_data1+1024),(uint8_t *)temp_b2,512);

SST25Write((add_data1+2048),(uint8_t *)temp_b4,512);

SST25Write((add_data1+2560),(uint8_t *)temp_b5,512);

SST25Write((add_data1+3072),(uint8_t *)temp_b6,512);

SST25Write((add_data1+3584),(uint8_t *)temp_b7,512);

blkc = 0;

 }

if(blkc == 5)

 {

SST25Write(a0,(uint8_t *)buf,512);

SST25Write((add_data1),(uint8_t *)temp_b0,512);

SST25Write((add_data1+512),(uint8_t *)temp_b1,512);

SST25Write((add_data1+1024),(uint8_t *)temp_b2,512);

SST25Write((add_data1+1536),(uint8_t *)temp_b3,512);

SST25Write((add_data1+2560),(uint8_t *)temp_b5,512);

SST25Write((add_data1+3072),(uint8_t *)temp_b6,512);

SST25Write((add_data1+3584),(uint8_t *)temp_b7,512);

blkc = 0;

 }

if(blkc == 6)

 {

SST25Write(a0,(uint8_t *)buf,512);

SST25Write((add_data1),(uint8_t *)temp_b0,512);

SST25Write((add_data1+512),(uint8_t *)temp_b1,512);

SST25Write((add_data1+1024),(uint8_t *)temp_b2,512);

SST25Write((add_data1+1536),(uint8_t *)temp_b3,512);

SST25Write((add_data1+2048),(uint8_t *)temp_b4,512);

SST25Write((add_data1+3072),(uint8_t *)temp_b6,512);

SST25Write((add_data1+3584),(uint8_t *)temp_b7,512);

blkc = 0;

 }

if(blkc == 7)

 {

SST25Write(a0,(uint8_t *)buf,512);

SST25Write((add_data1),(uint8_t *)temp_b0,512);

SST25Write((add_data1+512),(uint8_t *)temp_b1,512);

SST25Write((add_data1+1024),(uint8_t *)temp_b2,512);

SST25Write((add_data1+1536),(uint8_t *)temp_b3,512);

SST25Write((add_data1+2048),(uint8_t *)temp_b4,512);

SST25Write((add_data1+2560),(uint8_t *)temp_b5,512);

SST25Write((add_data1+3584),(uint8_t *)temp_b7,512);

blkc = 0;

 }

 if(blkc == 8)

 {

SST25Write(a0,(uint8_t *)buf,512);

SST25Write((add_data1),(uint8_t *)temp_b0,512);

SST25Write((add_data1+512),(uint8_t *)temp_b1,512);

SST25Write((add_data1+1024),(uint8_t *)temp_b2,512);

SST25Write((add_data1+1536),(uint8_t *)temp_b3,512);

SST25Write((add_data1+2048),(uint8_t *)temp_b4,512);

SST25Write((add_data1+2560),(uint8_t *)temp_b5,512);

SST25Write((add_data1+3072),(uint8_t *)temp_b6,512);

blkc = 0;

 }

 return (USBD_OK);

}

thanks in advance.

That does seem overly complex and convoluted. Is the erase size a sector or a sub-sector?

​

Can't you tell the systems you're using a 4KB block size.

You have stack space to accommodate this? Using GNU/GCC?​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
svii
Associate III

Hi thanks for the reply, the erase is the sector size which is 4K minimum for the flash erase operation, i did configure to use 4KB block size allocation but the system fails , it would have been easier if it had worked , hence tried to fix the size to 512 bytes allocation size .Sorry for the above code, didn't use any comments to follow,

what it does is to read ,erase , write a sector for 512 bytes with 4k erase without loosing the subsector data within the sector.Thanks in advance.

svii
Associate III

hi, the

a0 = add_blk * 512;   

a1 = blk_len * 1;

a0 is the address to the flash ie add_blk= 1; a0 =512.

a1 is the blk len should this multiplied by 512 else remain the same as above confused . Thanks

svii
Associate III

hi, thanks i was able to make the usb msc work ,created a folder wrote a text file and checked it.