Hello All, I am using STM32f105rbt, issue is comming when i am using Ethernet and PWM using TIM1 simualteniously. individually both are working. please any one can help me?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-09-04 11:35 PM
If i am generating PWM pulse by uing TIM1 (PA8) my ethernnet not worming?
for ethernet config i m using CMSIS lib provided by ST
Pwm configuration is s follows
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1, ENABLE);
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOA, &GPIO_InitStructure);
TIM_TimeBaseStructure.TIM_Prescaler = (uint16_t)(Prescaler);
TIM_TimeBaseStructure.TIM_Period = (uint16_t)(Period);
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseStructure.TIM_ClockDivision = 0; // Not used
TIM_TimeBaseStructure.TIM_RepetitionCounter = 0; // Not used
TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure);
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
TIM_OCInitStructure.TIM_Pulse = (uint16_t)(duty_cycle); // 50% /2
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_OutputNState = TIM_OutputNState_Enable;
//TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
//TIM_OCInitStructure.TIM_OCNPolarity = TIM_OCNPolarity_Low;
//TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Set;
//TIM_OCInitStructure.TIM_OCNIdleState = TIM_OCIdleState_Reset;
TIM_OC1Init(TIM1, &TIM_OCInitStructure);
TIM_Cmd(TIM1, ENABLE);
TIM_CtrlPWMOutputs(TIM1, ENABLE);
- Labels:
-
Ethernet
-
STM32F1 Series
-
TIM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-09-05 12:31 PM
STM32F105xx doesn't have Ethernet peripheral:
https://www.st.com/en/microcontrollers-microprocessors/stm32f105-107.html
There is no such thing as "CMSIS lib". Your code looks to be using the older SPL library.