cancel
Showing results for 
Search instead for 
Did you mean: 

Having trouble getting USB3300 to work with STM32F407

KK.2
Associate III

Hello there,

I've prototyped a custom PCB, but I'm having issues getting USB to work, Windows is unable to read the Device Descriptor.

The IO, from what I understand, is connected correctly and the generated code is (seemingly) successfully able to initialize the PHY, and the PC will only detect it as plugged in once the `USBD_Start` method within `MX_USB_DEVICE_Init` was executed thats generated by CubeMX.

Apart from having configured the Clocks and USB HS / Device (Com port example) it is a blank project

As the 3300 needs a 24MHz clock I've decided to configure it as shown here by using MCO2. My clock configuration looks like this: https://i.imgur.com/lAhx1jD.png

I've tried to simplify it by setting PLLI2S to x120 / 5 and thus have the MCO2 be /1 with no difference.

I've tried to switch to Full Speed over High Speed with no difference.

Any help would be appreciated, thank you.

This discussion is locked. Please start a new topic to ask your question.
21 REPLIES 21
KK.2
Associate III

Got a 24M crystal, swapped out the 25M one, changed the clocks so the HSE is passed trough aaand... Now I cant even get it to detect on Full Speed. Back to square one I guess.

Edit: Actually that was my fault, its the same behaviour as before now.

KK.2
Associate III

I'm slowly running out of things to try. Connected the 60MHz clkout line from the PHY to the STM with a jumper and cut the trace to prevent any possible crosstalk from that line, same result

I cut the only trace which goes across the board pretty much (ULPI data 7, because for whatever reason 0-6 are on the same side of the STM chip while 7 is on the complete opposite) and connected it with a jumper instead, same result

I painstakingly botched on a 24MHz crystal onto the PHY with its caps and resistor, same result.

Starting to wonder if all this time I've looked for a hardware bug while its just STM's implementation thats faulty. I also have a second board which confirmed that its not down to some broken component (Same problem)