cancel
Showing results for 
Search instead for 
Did you mean: 

Guys, can anyone recommend an STM chip that has more than 1 USB device interface? I'm trying to read data from PC (over USB) and send it to another device (over USB too at the same time )

JMANS.11
Associate
 
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Peter BENSCH
ST Employee

Yes, there are many of them, e.g. STM32F777, STM32H742, etc.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Uwe Bonnes
Chief

In stmcufinder click both USB OTH HS and FS. No phy needed if FS is enough for both.

but do they support HID protocol? and thanks so much