2025-12-29 3:52 AM - last edited on 2025-12-29 5:12 AM by mƎALLEm
Hello, dear colleagues!
If my request seems inappropriate to you, I apologise — but I had no other choice.
I've been struggling with this for a week now.
Please, if anyone has a ready-made working project, share it or give it to me.
I need a ready-made project for Nucleo-STM32H753ZI (MB1364-H753ZI-E01) that includes FreeRTOS with USB-CDC or Ethernet support.
I have tried many times, but I still cannot get past the FreeRTOS initialisation stage.
Thank you all.
*This post has been translated from Russian to comply with the ST Community guidelines.
Solved! Go to Solution.
2025-12-29 6:27 AM
Hello @boryabekk, and welcome to ST Community!
I have attached a freshly created and working project for the NUCLEO-H753ZI that features LwIP and FreeRTOS. You can use it as a starting point and add USB CDC after testing it. If you encounter any issues while running it, please let me know.
Best regards,
2025-12-29 5:06 AM - edited 2025-12-29 5:07 AM
Hello @boryabekk and welcome to the ST community,
For Ethernet+LWIP I suggest to refer to this knowledge base article, it uses already FreeRTOS: How to create a project for STM32H7 with Ethernet and LwIP stack working
2025-12-29 5:51 AM
First of all, thank you for your reply.
I have tried a lot using the resources you mentioned, but unfortunately, I still couldn’t get any successful result. I also tried many other sources, but in the end I realized that this work is beyond my current ability.
That’s why I hoped maybe someone could share a working project.
2025-12-29 5:54 AM - edited 2025-12-29 5:56 AM
Check also that example in CubeF7 package:
2025-12-29 6:27 AM
Hello @boryabekk, and welcome to ST Community!
I have attached a freshly created and working project for the NUCLEO-H753ZI that features LwIP and FreeRTOS. You can use it as a starting point and add USB CDC after testing it. If you encounter any issues while running it, please let me know.
Best regards,
2025-12-30 6:10 AM
Hi @boryabekk
This example may be helpful as well.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.