cancel
Showing results for 
Search instead for 
Did you mean: 

Ethernet DMA status enter state TPS 010 for indefinite time

victor
Associate
Posted on September 23, 2013 at 15:48

I'm trying to use LwIP stack. I've set the PHY to advertise for 10M half duplex and autonegociation on. All registers of interest MAC, PHY and DMA are recorded into flash for monitoring purposes. After ethernet configuration hello_init a arp gratuition is sent and then arp queries at every 5 s. However the ethernet frame is never sent on phy. After netif->linkoutput is called the DMA status stays at : 00260400. (transmit waiting for status). Time stamp is not set and the configuration regs are:

MAC Configuration      -0000A40C

DMA Bus Mode:          -02820100

DMA Operation Mode -07202042

Interrupt Enable            -00010040

While TDES0               -B0D00000

          RDES0               -80000000

Thanks in advance for any help provided.

#stm32comstick-ethernet-driver
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0