Does the STM32F303 USB require an external termination series resistor?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-05-11 4:12 AM
In the STM32F303 datasheet is written that "no external termination series resistor are required on USB_D+ and USB_D-, the matching impedance is already included in the embedded driver." However, if I look at the STM32F3DISCOVERY board I see 22 Ohm termination series resistors before the CN2 (USB-USER connector).Do I need them in my design or not? Is it necessary also to design the signal traces in the PCB in order to show a particular characteristic impedance?
Labels:
- Labels:
-
STM32F3 Series
-
USB
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0