2019-07-23 11:20 AM
When generating code for the STM32L051C8Tx and STM32L053C8Tx MCUs using CubeMX I am experiencing a build error when setting channel 1 of TIM21 in input capture mode. The following line is added in main.c within the void SystemClock_Config(void) function because the input capture is assigned to the PB13 pin:
HAL_RCC_MCOConfig(RCC_MCO3, RCC_MCO1SOURCE_SYSCLK, RCC_MCODIV_1);RCC_MCO3 is not defined and this causes a compilation error. This macro is defined within stm32l0xx_hal_rcc.h, but is not included because the L051 and L053 are not listed.
#if defined(STM32L031xx) || defined(STM32L041xx) || defined(STM32L073xx) || defined(STM32L083xx) || defined(STM32L072xx) || defined(STM32L082xx) || defined(STM32L071xx) || defined(STM32L081xx)
#define RCC_MCO3 ((uint32_t)0x00000002)
#endifSimilar problem here in the same file:
#if defined(STM32L031xx) || defined(STM32L041xx) || defined(STM32L073xx) || defined(STM32L083xx) || defined(STM32L072xx) || defined(STM32L082xx) || defined(STM32L071xx) || defined(STM32L081xx)
#define IS_RCC_MCO(__MCO__) (((__MCO__) == RCC_MCO1) || ((__MCO__) == RCC_MCO2) || ((__MCO__) == RCC_MCO3))
#else
#define IS_RCC_MCO(__MCO__) (((__MCO__) == RCC_MCO1) || ((__MCO__) == RCC_MCO2))
2019-07-31 7:11 AM
Hello @SPetr.6 ,
Thanks for reporting this issue.
I confirm this issue from my side, and raised it internally to the appropriate teams for fix.
Thank for your contribution.
Kind Regards,
Imen