cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H753 HSE Not Generating Clock with NX2016SA crystal

SRAravind2410
Visitor

Hi Team,

     I’m currently working on a project using the NX2016SA 25 MHz crystal resonator from NDK
(Datasheet: https://www.ndk.com/images/products/catalog/c_NX2016SA_e.pdf).

All configurations have been done through STM32CubeIDE , and the setup is as follows:

Step 1: IOC Configuration

  • Enabled High-Speed External (HSE) clock.
  • Selected Crystal/Ceramic Resonator mode.
  • Enabled PH0 (RCC_OSC_IN) and PH1 (RCC_OSC_OUT) in the pinout.

Step 2: Clock Configuration

  • In the Clock Configuration tab:
  • Set HSE as the PLL input.
  • Used the “Resolve Clock Issues” option to fix initial PLL setup errors.

Step 3: Code Generation and Flash

  • Code was successfully generated and flashed to the board.
  • No compilation or linking errors.
  • The microcontroller powers on as expected.

Issue Observed

  • When probing PH0 and PH1 using a DSO (Digital Storage Oscilloscope), no clock waveform is observed.
  • The crystal does not appear to be oscillating.
  • There is no sign of activity or ringing — both lines are flat.

Step 4: Hardware (Schematic)

  • Crystal: NX2016SA-25M connected to PH0 and PH1.
  • Two 10 pF load capacitors connected from each crystal pin to GND.
  • Pads 2 and 4 of the crystal are connected to GND (as per datasheet recommendation).

Additional Notes

  • The project setup was done directly using STM32CubeIDE.
  • Target MCU: STM32H753VIT6 (100-pin LQFP).
  • VCAPs, VDD, and other power lines are confirmed stable.

 

Request

Could you please help identify potential reasons why the crystal oscillator is not functioning?

Possible areas for guidance:

  • Is any additional RCC or PWR configuration needed manually in code for STM32H7 series?
  • Does HSE require any delay or stabilization time in startup code?
  • Could the load capacitors (10 pF) be too low or too high for this crystal?
  • Should the internal bypass resistor or drive strength be configured?

Please let me know if any additional details such as full schematic, startup code, project are needed.

 

Screenshot (303).png

 

 

 

Thanks & Regards,

Aravind.SR

 

0 REPLIES 0