cancel
Showing results for 
Search instead for 
Did you mean: 

Can the STUSB4761 as a standalone device perform a DR_Swap?

SDick.1
Associate

We have an application that's currently using a USB BC1.2 IC to enumerate a charge condition (CDP) between a USB-u sinking host and a sourcing device. We're looking to add an IC between the existing circuit acting as the sourcing device and a USB-C device that would allow for the USB-C device to become the sinking DFP. If the USB-C peripheral starts out as a sinking UFP and initiates a DR_SWAP command, will the STUSB4761 be able to complete the sequence for the data role swap and allow the USB-C peripheral to act as a sinking DFP? Can this be done with only the STUSB4761, without the need for any other external memory, MUX, etc?

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
NBALL
ST Employee

​Hello,

If STUSB4761 receives DR_SWAP from th SINK, it will accept it and will swap datarole in its capabilities.

Regards,

PVala.1
Associate II

Hi SDick.1

Have you checked this functionality by STUSB4761 as we also want to use this chipset in same type of application ?

Device mode with source power to other device .

SDick.1
Associate

Hello,

Our application required the opposite of what you're asking, but I would imagine this IC would provide the handshake needed if what you're connecting to already has the capability to do so on its end.

Sam

NBALL
ST Employee

​Hello

By default stusb4761 accepts all DR_swap messages.

Thus it becomes a sourcing UFP for the counterpart.

Regards