Azure RTOS: function "tx_event_flags_get" does not react if it waits too long
- June 23, 2023
- 1 reply
- 2395 views
Hello everyone,
on my Evalboard (STM32H750B-DK) I use Azure RTOS, NetX Duo and the MQTT stack. I run the RTOS with two threads. The first thread (low priority) is the heartbeat thread. In this thread, only one LED is blinking. In the second thread (high priority) a MQTT communication is running. Sending and receiving works also very well.
About the problem: I have the problem that the function "tx_event_flags_get()" does not always react to the event. It almost never reacts to the event if the event occurs after a certain time ( approx. longer than 20 seconds). The event that is waited for is an MQTT message.
If the µC reaches the above mentioned function and then the event occurs immediately after 1-2 seconds, then everything works very well.
How can it be that when the µC spends a longer time in the "tx_event_flags_get" function, it stops responding to the event even when the event actually arrives?
The relevant code looks like the following. I have added the full code as a text file to the attachment. If you need any additional information beyond that, please let me know:
/* Includes ------------------------------------------------------------------*/
#include "app_netxduo.h"
#include "nxd_mqtt_client.h"
#include "main.h"
#include "string.h"
#include "stdio.h"
/* Private define ------------------------------------------------------------*/
#define LOCAL_SERVER_ADDRESS (IP_ADDRESS(192,168,0,14))
#define MQTT_CLIENT_STACK_SIZE 4096
#define CLIENT_ID_STRING "mytestclient"
#define STRLEN(p) (sizeof(p) - 1)
#define SUB_TOPIC_NAME "Temp/Sensor/Value/f"
#define MQTT_THREAD_PRIORTY 2
#define MQTT_KEEP_ALIVE_TIMER 300
#define QOS0 0
#define QOS1 1
#define DEMO_MESSAGE_EVENT 1
#define DEMO_ALL_EVENTS 3
/* Private variables ---------------------------------------------------------*/
TX_THREAD NxAppThread;
TX_THREAD NxHbThread;
NX_PACKET_POOL NxAppPool;
NX_IP NetXDuoEthIpInstance;
NXD_MQTT_CLIENT mqtt_client;
TX_EVENT_FLAGS_GROUP mqtt_app_flag;
static ULONG mqtt_client_stack [MQTT_CLIENT_STACK_SIZE / sizeof(ULONG)];
static UCHAR message_buffer [NXD_MQTT_MAX_MESSAGE_LENGTH];
static UCHAR topic_buffer [NXD_MQTT_MAX_TOPIC_NAME_LENGTH];
char* MESSAGE_STRING = "";
/* Private function prototypes -----------------------------------------------*/
static VOID nx_app_thread_entry (ULONG thread_input);
static VOID nx_app_hb_entry (ULONG thread_input);
static VOID my_notify_func(NXD_MQTT_CLIENT* client_ptr, UINT number_of_messages)
{
tx_event_flags_set(&mqtt_app_flag, DEMO_MESSAGE_EVENT, TX_OR);
return;
}
static VOID nx_app_thread_entry (ULONG thread_input)
{
UINT ret = NX_SUCCESS;
NXD_ADDRESS server_ip;
ULONG events;
UINT topic_length
UINT message_length;
UINT i = 0;
/* Create MQTT client instance. */
ret = nxd_mqtt_client_create(&mqtt_client, "my_client", CLIENT_ID_STRING, STRLEN(CLIENT_ID_STRING), &NetXDuoEthIpInstance, &NxAppPool,(VOID*)mqtt_client_stack, sizeof(mqtt_client_stack MQTT_THREAD_PRIORTY, NX_NULL, 0);
/* Create an event flag for this demo. */
tx_event_flags_create(&mqtt_app_flag, "my app event");
/*Select the IP protocol version and the IP address of the broker*/
server_ip.nxd_ip_version = 4;
server_ip.nxd_ip_address.v4 = LOCAL_SERVER_ADDRESS;
/* Start the connection to the server. */
ret = nxd_mqtt_client_connect(&mqtt_client, &server_ip, NXD_MQTT_PORT, MQTT_KEEP_ALIVE_TIMER, 0, NX_WAIT_FOREVER);
/* Subscribe to the topic with QoS level 0. */
ret = nxd_mqtt_client_subscribe(&mqtt_client, SUB_TOPIC_NAME, STRLEN(SUB_TOPIC_NAME), QOS0);
/* Set the receive notify function. */
ret = nxd_mqtt_client_receive_notify_set(&mqtt_client, my_notify_func);
while(1)
{
/*Wait until MQTT message has arrived*/
tx_event_flags_get(&mqtt_app_flag, DEMO_ALL_EVENTS, TX_OR_CLEAR, &events, TX_WAIT_FOREVER);
/* Let the LED blink 10 times to signal the receipt of a new MQTT message */
do
{
HAL_GPIO_TogglePin(GPIOJ, GPIO_PIN_2);
tx_thread_sleep(10);
i++;
} while(i<10);
i = 0;
/* Get the receiving MQTT message */
if(events & DEMO_MESSAGE_EVENT)
{
ret = nxd_mqtt_client_message_get(&mqtt_client, topic_buffer, sizeof(topic_buffer), &topic_length, message_buffer,sizeof(message_buffer), &message_length);
}
if(message_buffer[0] == "X")
{
break;
}
}
/* Now unsubscribe the topic. */
nxd_mqtt_client_unsubscribe(&mqtt_client, SUB_TOPIC_NAME, STRLEN(SUB_TOPIC_NAME));
/* Disconnect from the broker. */
nxd_mqtt_client_disconnect(&mqtt_client);
/* Delete the client instance, release all the resources. */
nxd_mqtt_client_delete(&mqtt_client);
/* USER CODE END Nx_App_Thread_Entry 0 */
}
static VOID nx_app_hb_entry (ULONG thread_input)
{
while(1)
{
HAL_GPIO_TogglePin(GPIOI, GPIO_PIN_13);
tx_thread_sleep(30);
}
}
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */