cancel
Showing results for 
Search instead for 
Did you mean: 

ADC_STm32G0

meena
Associate III

hi..I have tried all the ways to read ADC values as I found that using PA11(ADC_IN15) and PA12(ADC_IN16) is the issue.I tried setting up non configured mode  with polling and also DMA (as per CubeG0 examaples) I couldnt able to read the values. Can any one help with this please.

To confirm this Out of 7 channels I needed I tried with 5 channels sequencer fully configuarable mode and that works fine if I add these two channelsPA11(ADC_IN15) and PA12(ADC_IN16) I am getting same values for all the channels

 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
STea
ST Employee

Hello @meena ,

depending on the package (LQFP48/UFQFPN48) and according to datasheet table 12 you can use PA11 and PA12 

for ADC_IN15 and ADC_IN16 respectively with pin  PB11 and PB12 this is already reported internally as a typo in the datasheet so PB11,PB12 are only available for ADC_15,ADC_16 .

This typo will be fixed in the next revision .

BR

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.