cancel
Showing results for 
Search instead for 
Did you mean: 

Accessing HAL TIM struct fields pointers inside other structs correctly.

Posted on April 25, 2017 at 12:21

I have the following structs (from a library I'm using) with some fields and I would like to assign with OR operation a new value. But I'm debugging and I can't see how anything is writing there:

typedef struct { 
TIM_TypeDef *Instance; /*!< Register base address */ 
TIM_Base_InitTypeDef Init; /*!< TIM Time Base required parameters */ 
HAL_TIM_ActiveChannel Channel; /*!< Active channel */ 
DMA_HandleTypeDef *hdma[7]; /*!< DMA Handlers array This array is accessed by a @ref DMA_Handle_index */
HAL_LockTypeDef Lock; /*!< Locking object */ 
__IO HAL_TIM_StateTypeDef State; /*!< TIM operation state */
}TIM_HandleTypeDef; 
typedef struct
{ 
__IO uint32_t CR1; /*!< TIM control register 1, Address offset: 0x00 */
__IO uint32_t CR2; /*!< TIM control register 2, Address offset: 0x04 */
__IO uint32_t SMCR; /*!< TIM slave mode control register, Address offset: 0x08 */ 
__IO uint32_t DIER; /*!< TIM DMA/interrupt enable register, Address offset: 0x0C */ 
__IO uint32_t SR; /*!< TIM status register, Address offset: 0x10 */ 
__IO uint32_t EGR; /*!< TIM event generation register, Address offset: 0x14 */ 
__IO uint32_t CCMR1; /*!< TIM capture/compare mode register 1, Address offset: 0x18 */ 
__IO uint32_t CCMR2; /*!< TIM capture/compare mode register 2, Address offset: 0x1C */ 
__IO uint32_t CCER; /*!< TIM capture/compare enable register, Address offset: 0x20 */ 
__IO uint32_t CNT; /*!< TIM counter register, 
 ... 
} TIM_TypeDef;

I have a part of code where I defined:

 TIM_HandleTypeDef TIMER_Struct;

And I would like to access the field 'CR1' of TIM_TypeDef struct that is '*Instance' field of TIM_HandleTypeDef. So I have done it by this way in a function:

 void DRV_TIMER_init(void) 
{ 
... 
TIMER_Struct.Instance = TIMx;//TIM7
TIMER_Struct.Init.Period = 100 - 1; 
TIMER_Struct.Init.Prescaler = uwPrescalerValue; 
TIMER_Struct.Init.ClockDivision = 0; // these accesses work 
TIMER_Struct.Instance -> CR1 |= 0x01 << 3; // this no works 
... 
}

Even if I write directly:

 TIMER_Struct.Instance -> CR1 = 0xFFFFFFFF; 

It stills without having effect.

I think It could be a fact that I'm not controlling appropiately the pointer access or similar. But I don't see how can I access and modify the content of the commented field. Since I can see (debug mode) how the rest of struct fields updates are writen correctly.

Any correction suggested here?

TIMER_Struct.Instance -> CR1 = 0xFFFFFFFF; 

I try different ways to get it with no success. I need new ideas. How would you do if you want write there?

Thanks in advance.

#pointers #hal-tim-structs
This discussion is locked. Please start a new topic to ask your question.
13 REPLIES 13
Posted on April 26, 2017 at 13:09

no, there is no difference in the case of this register.

Posted on April 26, 2017 at 13:34

Thanks for the clarification, Max!!!

David.Yves
Associate II
Posted on April 27, 2017 at 12:27

I think there is precedence involved:

your instruction could be    TIMx->CR1 =(TIMx-> CR1 |  0x1) <<3;

or it could be                      TIMx->CR1 =TIMx-> CR1 |  (0x1 <<3);

I believe you want the latter one  and since 1<<3 is 8

try this      TIMx->CR1 |=8;       in your case   

Instance

->

CR1

|=

8

;

if this works  let me know

if not sorry for wasting your time

Yves

Posted on April 27, 2017 at 15:13

Hi David, Yes second one. I think you are all right and your idea is more exact than the first one. When you have a register with a concret value and you don't want modify the rest of bits except one, the best solution is your second one. The first one only will be correct if I have all 0x00. If not I will be shifting the rest of bits and I don't want this. 

Am I wrong?