cancel
Showing results for 
Search instead for 
Did you mean: 

3 SPI busses does not parallelize data access

rlegault
Associate II

STM32H743
We have 4 SPI busses running at 12.5MHz but the SPI clocks are sequentially. SPI 1 and 2 are using DMA Channel 1 while SPI 3 and 4 are using DMA Channel 2. We would like them to run in parallel.
Can they run in parallel.

The code uses HAL_SPI_TransmitReceive_DMA() for each of the calls to the spi to Tx and Rx.The picture below definitely shows serialization of the accesses. Each access is 32 bytes.

rlegault_0-1705436036380.png

The picture above shows the clocks of 3 of the spi busses and it is quite evident that the SPI busses are not running in parallel.

1 ACCEPTED SOLUTION

Accepted Solutions
rlegault
Associate II

The SPI accesses were ending before the next one could be setup decreasing the clock frequency shows them running in parallel.

3spi_in_parallel.png

 

View solution in original post

1 REPLY 1
rlegault
Associate II

The SPI accesses were ending before the next one could be setup decreasing the clock frequency shows them running in parallel.

3spi_in_parallel.png