Why my MCU is not detected
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-09-22 6:42 PM
In the picture:
pin 1 top left: VDD 3.3V
4 100n to GRND
14 to GRND
15 to VDD
16 to GRND
on their left 1µ and 10n F decoupling VDDA VSSA
pin 32 top right : VSS 0V GRND
pin 31 10K ohm to GRND
24 SWD clk
23 SWD dio
17 to GRND
top left and bottom right 100nF decoup. PWRS + the blue one 4.7µF
tried many combinations: with the reset on/off , boot0 on/off, swapped 23/34 ,
the ideMXcube and the standalone programmer wont see the MCU:
target not found,
ps: the red LED in ON .
my stlink v2 works in this setup with: another nucleo G4 and the generic "blue pill" fine.
Any help or suggestions ?
Thank you in advance.
- Labels:
-
STM32G4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-09-22 7:10 PM
Lack of any markings, are you sure this is a functional part.
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
2022-09-22 8:17 PM
I have just got three of these from farnell, the soldered one got too much flux ... :)
photo attached.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-09-22 9:45 PM
FYI, to solder the SMD, I used glue to hold the chip in place.
I didnt use wood glue, especially not superglue,
but paper glue, like we use in class rooms.
So my thought is that this glue has a resistance, maybe pins are shortcut-ted underneath,
I have just mesured the resistance of the glue, it is about 0.3 Mohm -> 300Kohm .
And yet the LED lights up .
I will retest after a while (more dried glue)
And then will try to clean up underneath the chip ...
Regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-10-03 9:55 AM
Made another board, this time, no glue and no overheat, I soldered so quickly , I held the chip with my finger and didn't get burned ...
my question, BTW:
Am I missing the quartz ? because I taught, this chip can start with its own RC clock ...
Also, I am powering up the board with stlink2 's 3.3v , yes the stlink is a clone ...
Regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-10-03 11:07 AM
The STM32 typically start from HSI or MSI, you have to manually start the HSE external one.
The secondary signs-of-life is sending the 0x7F data pattern via UART into the system loader. See AN2606, and AN3155
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
2022-10-03 11:10 AM
>this chip can start with its own RC clock.
right so.
you should see the clock tree in Cube or STM32cubeIDE ...right?