STM32l412 Nucleo-32 Dev Board has shorted pins?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-04-28 11:36 AM
The following pins appear to be shorted on the STM32L412 Nucleo-32 Dev Board :
A4 (PA5) shorted to D4 (PB7)
and
A5 (PA6) shorted to D5 (PB6)
Is it possible someone can verify, I have checked four Nucleo-32 boards and all show the shorted pins. The Nucleo board also does show this shorted behavior when powered up in the system.
Labels:
- Labels:
-
STM32L4 series
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-04-28 11:55 AM
OK, never mind, I downloaded the gerbers and found that there are 0ohm resistors connecting these pins. I am sure it is documented somewhere. Seems kinda odd.