cancel
Showing results for 
Search instead for 
Did you mean: 

STLink-V3PWR: How to identify COM Port

lmessing
Associate II

I am struggling to find a good way to identify the two COM ports the STLink-V3PWR provides. One is for direct communication with the power measurement unit and the other is connected to DEBUG for the target device(VCP).

We need a easy way to identify the DEBUG UART port of the STLink-V3PWR. When performing the "-l uart" command with the STM32_Programmer_CLI.exe we receive two identical outputs for both ports. This is not the case with the STLINK-V3SET, because we get an easy identifyable description "STMicroelectronics STLink Virtual COM Port". 

In the example below, how do I distinguish between COM20 and COM21? There must be a better way than opening both ports and checking which one responds to the "version" command.

Example Outputs:

STLINK-V3SET

"C:\\Program Files\\STMicroelectronics\\STM32Cube\\STM32CubeProgrammer\\bin\\STM32_Programmer_CLI.exe" -l uart
-------------------------------------------------------------------
STM32CubeProgrammer v2.14.0
-------------------------------------------------------------------

===== UART Interface =====

Total number of serial ports available: 1

Board Name : STLINK-V3SET
ST-LINK SN: 0047001D3037510339373532
Port: COM4
Location: \\.\COM4
Description: STMicroelectronics STLink Virtual COM Port
Manufacturer: STMicroelectronics

STLINK-V3PWR

"C:\\Program Files\\STMicroelectronics\\STM32Cube\\STM32CubeProgrammer\\bin\\STM32_Programmer_CLI.exe" -l uart
-------------------------------------------------------------------
STM32CubeProgrammer v2.14.0
-------------------------------------------------------------------

===== UART Interface =====

Total number of serial ports available: 2

Board Name : STLINK-V3PWR
ST-LINK SN: 002300433432511839383236
Port: COM20
Location: \\.\COM20
Description: Serielles USB-Gerõt
Manufacturer: Microsoft

Board Name : STLINK-V3PWR
ST-LINK SN: 002300433432511839383236
Port: COM21
Location: \\.\COM21
Description: Serielles USB-Gerõt
Manufacturer: Microsoft

 

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10

Installing the driver fixes this issue, thank you!

-l uart shows now a good description as well:

Board Name : STLINK-V3PWR
ST-LINK SN: 002300433432511839383236
Port: COM20
Location: \\.\COM20
Description: STMicroelectronics STLink Virtual COM Port PWR
Manufacturer: STMicroelectronics

Board Name : STLINK-V3PWR
ST-LINK SN: 002300433432511839383236
Port: COM21
Location: \\.\COM21
Description: STMicroelectronics STLink Virtual COM Port
Manufacturer: STMicroelectronics

Would be great if this driver was installed automatically when installing STM32CubeMonitor-Power or STM32CubeProgrammer.