cancel
Showing results for 
Search instead for 
Did you mean: 

ST-Link Utility setup.

kvresto
Senior

Hi. I have setup st-link utility to start from within cubeide, but now I want to know how to make the utility start in the directory of my project where the .hex file is located, so I don't have to dig into the file system manually. I have attached an image of progress so far.

Thanks.

EDIT: With ac6 you could program the target from within the ide, is this also possible with cube ide.

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Pavel A.
Super User

> With ac6 you could program the target from within the ide, is this also possible with cube ide.

Yes, possible,

-- pa

kvresto
Senior

thanks, Pavel. can this be done without using st-link utility?

kvresto
Senior

any "constructive" argument that will work?

Pavel A.
Super User

In a recent CubeIDE version something has been added to download program to the target, without debugging (though this is actually done via debugger)

-- pa

kvresto
Senior

onya captain, your a marvel.