Skip to main content
Visitor II
December 23, 2024
Question

Simple Upload Firmware By Customer using dapboot

  • December 23, 2024
  • 0 replies
  • 689 views

Good morning everyone,

I'm here to ask for advice regarding the approach I want to take for enabling firmware updates by non-expert users.

I have built hardware that uses the STM32F103, and over time I will certainly release updates. Currently, I'm using a serial interface for uploads, but I would like to simplify the process further (avoiding the need to move the BOOT0 switch to + or use USB-UART converter chips).

I'm studying the DFU upload method and have tried various bootloaders. I found one called dapboot, which is quite appealing because when you connect the USB, it opens the DFU web interface to upload the firmware directly.

The problem is that I can't integrate it with my sketch written using PlatformIO and the Arduino framework.

I want my program sketch to trigger the dapboot bootloader using a specific button combination. If this combination is not pressed, the program should run the main application sketch instead.

I've tried writing to two different memory addresses, but I lack the skills to manage the two types of startup.

Can anyone help me?
Thank you!

This topic has been closed for replies.