2025-09-28 10:44 PM
Hi, I am currently working on a custom board design based on the STM32N657X0H3Q microcontroller. To ensure correct implementation and speed up the design process, I would like to study the reference Altium design projects of ST’s official boards.
Specifically, I am looking for the Altium project/source design files (schematics + PCB) for the following boards:
STM32N6570-DK (STM32N6 Discovery Kit)
NUCLEO-N657X0-Q (STM32N6 Nucleo-144 Board)
The PDFs of the schematics are available, but having access to the full Altium project files would help me greatly in understanding layout practices, power distribution, signal routing, and peripheral connections.
Could you please guide me on how I can obtain these design files?
Solved! Go to Solution.
2025-09-28 11:41 PM - edited 2025-09-28 11:42 PM
Hello @GBA
I suggest you have a look at the « Board design project» .zip files available here for the STM32N6570-DK board and here for the NUCLEO-N657X0-Q.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-09-28 11:41 PM - edited 2025-09-28 11:42 PM
Hello @GBA
I suggest you have a look at the « Board design project» .zip files available here for the STM32N6570-DK board and here for the NUCLEO-N657X0-Q.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.