cancel
Showing results for 
Search instead for 
Did you mean: 

ODR rate on ISM330DHCXTR

DDineshkumar
Associate II

Hello,

 

I'm using (ISM330DHCXTR) accelerometer to calculate the phase difference between two axes to measure the movement of a system. configured ODR at 6.6 KHz and measured the operation frequency of the system which has a 10% error while measuring the FFT and adjusted the ODR on the math lab logic to match the operation frequency of the system but still the phase difference has a major deviation, can someone confirm what is the ODR deviation on this sensor and how to correct the same on the firmware instead of modifying on the paired application.

 

 

0 REPLIES 0