2025-12-19 4:19 PM
I’m attempting to learn BLE and IoT and have purchased the following boards to get started.
NUCLEO-F401RE MCU brd
X-NUCLEO-IDB05A2 BLE Expansion brd
Downloaded:
STM32CubeIDE Version: 2.0.0 Build: 26820_20251114_1348 (UTC)
STM32CubeMX Version: 6.16.1
x-cube-ble1 BLE Demo
The main program calls HAL-Init() which goes directly to the HardFault_Handler()
My preliminary conclusion is that Version 20.0.0 is not compatible with the demo program based on help I sought on ChatGPT. It recommends Version 1.19.0. Is this correct?
May need to back up and start from scratch and would appreciate a point in the right direction to avoid going down any unnecessary rabbit holes.
Thank you, BareMetaler