cancel
Showing results for 
Search instead for 
Did you mean: 

No data-role swap recognized with X Cube TCPP

chris_O
Associate

Hello,

 

I am using a STM32G0B1xx MCU with the X-CUBE-TCPP v4.1.0 stack an FreeRTOS. I am trying to setup a USB-c port with OTG-functionality. I am having some problems understanding your X-CUBE-TCPP-stack.

Some background info:

I am initializing the software with MX_UCPD1_Init() and MX_USBPD_Init() provided by the original stack/CubeMX. I am testing the connection with several USB-devices an -hosts.  We tested a previous version of our software on a  NUCLEO-G071RB in combination with a X-NUCLEO-DRP1M1 with your Tool "STM32CubeMonitor-UCPD", which was working fine.

 

1. The DPM_Params[0].PE_DataRole is always defined as USBPD_PORTDATAROLE_UFP, no matter what i connect to the USB-c port. Is this intended?

 

2. I do not get a Notification for USBPD_NOTIFY_DATAROLESWAP_UFP or for USBPD_NOTIFY_DATAROLESWAP_DFP in here, no matter what I connect to the USB-c port:

/**
  * @brief  Callback function called by PE to inform DPM about PE event.
  * @PAram  PortNum The current port number
  * @PAram  EventVal @ref USBPD_NotifyEventValue_TypeDef
  * @retval None
  */
void USBPD_DPM_Notification(uint8_t PortNum, USBPD_NotifyEventValue_TypeDef EventVal)
{
/* USER CODE BEGIN USBPD_DPM_Notification */
  /* Manage event notified by the stack? */
  switch(EventVal)
  {
//...
    case USBPD_NOTIFY_DATAROLESWAP_UFP:
    	HAL_NVIC_SetPendingIRQ(EXTI2_3_IRQn); // this will set EVENT_DATAROLE_CHANGE
    	break;
    case USBPD_NOTIFY_DATAROLESWAP_DFP:
    	HAL_NVIC_SetPendingIRQ(EXTI2_3_IRQn); // this will set EVENT_DATAROLE_CHANGE
    	break;
    default:
      DPM_USER_DEBUG_TRACE(PortNum, "ADVICE: USBPD_DPM_Notification:%d", EventVal);
      break;
  }
/* USER CODE END USBPD_DPM_Notification */
}

I just get  two notification in the beginning, both USBPD_NOTIFY_USBSTACK_START.

 

Do you have any hints for me where to start?

 

1 REPLY 1
FBL
ST Employee

Hi @chris_O 

USBPD and USB stack run in parallel. If we see that the data role swap is done in the USBPD trace (UCPD monitor) it doesn't mean that the USB stack is in the right state. Here is the default the USB role when attached.

To be sure that the USB stack role is aligned with USBPD status, See the wiki.

A notification system is in place for USBPD stack to notify USB part :

void USBPD_DPM_Notification(uint8_t PortNum, USBPD_NotifyEventValue_TypeDef EventVal)
{
  switch(EventVal)
  {
    case USBPD_NOTIFY_USBSTACK_START:
    {
	if (USBPD_PORTDATAROLE_DFP == DPM_Params[PortNum].PE_DataRole)
	{
	  USBPD_USBIF_HostStart(PortNum);
	}
	else
	{
	  USBPD_USBIF_DeviceStart(PortNum);
	}
	break;
    }
    case USBPD_NOTIFY_USBSTACK_STOP:
    {
	 if (USBPD_PORTDATAROLE_DFP == DPM_Params[PortNum].PE_DataRole)
	 {
	  USBPD_USBIF_HostStop(PortNum);
	 }
	 else
	 {
	  USBPD_USBIF_DeviceStop(PortNum);
	 }
	 break;
  }
   case USBPD_NOTIFY_DATAROLESWAP_DFP :
   {
    USBPD_USBIF_Swap2Host(PortNum);
    break;
   }
  case USBPD_NOTIFY_DATAROLESWAP_UFP :
  {
    USBPD_USBIF_Swap2Device(PortNum);
    break;
  }
}
  1.  

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.