cancel
Showing results for 
Search instead for 
Did you mean: 

Necleo-STM32F767ZI board fails on example "LwIP_HTTP_Server_Netconn_RTOS"

Chao
Senior II

Hi,

I just bought a Necleo-STM32F767ZI board, and downloaded the example "LwIP_HTTP_Server_Netconn_RTOS" in CubeIDE, and made following changes in main.h:

#define IP_ADDR2   3

#define GW_ADDR2 3

As for the board, I did not make any changes on the jumpers.

then built it and ran it, I saw the LEDs changes, but it failed almost immediately after file-download-complete. The following are the texts shown in the console window:

 

STMicroelectronics ST-LINK GDB server. Version 7.5.0

Copyright (c) 2023, STMicroelectronics. All rights reserved.

 

Starting server with the following options:

Persistent Mode : Disabled

Logging Level : 1

Listen Port Number : 61234

Status Refresh Delay : 15s

Verbose Mode : Disabled

SWD Debug : Enabled

InitWhile : Enabled

 

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

-------------------------------------------------------------------

STM32CubeProgrammer v2.15.0

-------------------------------------------------------------------

 

Log output file: C:\Users\15023\AppData\Local\Temp\STM32CubeProgrammer_a19868.log

ST-LINK SN : 066CFF485753667187172243

ST-LINK FW : V2J43M28

Board : NUCLEO-F767ZI

Voltage : 3.22V

SWD freq : 4000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID : 0x451

Revision ID : Rev Z

Device name : STM32F76x/STM32F77x

Flash size : 2 MBytes

Device type : MCU

Device CPU : Cortex-M7

BL Version : 0x93

 

Memory Programming ...

Opening and parsing file: ST-LINK_GDB_server_a19868.srec

File : ST-LINK_GDB_server_a19868.srec

Size : 117.27 KB

Address : 0x08000000

 

Erasing memory corresponding to segment 0:

Erasing internal memory sectors [0 3]

Download in Progress:

 

File download complete

Time elapsed during download operation: 00:00:02.298

 

Verifying ...

 

Download verified successfully

 

Shutting down...

Exit.

 

 

Anyone knows wher the problem is?

 

Regards

Chao

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @Chao 

I can't find any problem on the message you just shared. The code has been succesfully downloaded and the:

" Shutting down... Exit."

Means the end of the download operation.

For the printf fonction, you can use it on this board since it have a virtual com port. Al you have is to do the necessary coding and configurations.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5
Chao
Senior II

Is it possible to use printf to print debug messages to the console window in this example?

TDK
Super User

The log file looks fine to me.

> it failed almost immediately after file-download-complete

In what way specifically did it fail?

If you feel a post has answered your question, please click "Accept as Solution".
STTwo-32
ST Employee

Hello @Chao 

I can't find any problem on the message you just shared. The code has been succesfully downloaded and the:

" Shutting down... Exit."

Means the end of the download operation.

For the printf fonction, you can use it on this board since it have a virtual com port. Al you have is to do the necessary coding and configurations.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

OK, thanks. I do be misled by the message "Shutting down... Exit.".

Now it works when I comment out the "#define LWIP_DHCP  1"

I will try to make printf work next.

Regards

Chao

I started a new project with selected target of Nucleo-STM32F767ZI board, and followed the instructions from 

"How to redirect the printf function to a UART for debug messages"

The printf works in the new project, however, when I did the same in the example project "LwIP_HTTP_Server_Netconn_RTOS", I did not get anything from printf. I added the following into the main.c of the example project:

Chao_0-1707067625285.png

and 

 

Chao_1-1707067726651.png

Regards

Chao