2025-03-09 12:35 PM
I am using a small outrunner motor to try to use Motor Profiler.
When I select Start Profile, it times out as shown in screen below. I have only enabled Potentiometer feature.
The pole pairs is 11, and the snapshot below shows max speed also changed to a lower value of 4000 since the default of 16000 also did not work. I also lowered max current to 20 A, but of no use.
Since I could not get Profiler to work, I tried to spin the motor after closing the Profiler. Changing potentiometer settings ( from low to high) did not spin the motor. I then enabled ESC and disabled the potentiometer feature, regenerated the code, built and programmed the board. Using an Arduino board, I generated a PWM signal with a period of 490 hz and high time of 1218 us, which should have armed and start spinning the motor, but nothing happens according to the user manual.
I want to check that the kit that I got is working.
Any help would be greatly appreciated.