cancel
Showing results for 
Search instead for 
Did you mean: 

H743, F765 & F429 MCUs with UFBGA176+25 (10 x 10 mm) IC package pin-out & cost comparisons

S.Kamath
Associate III

We're evaluating STM32 controllers in our product. We have shortlisted the following 3 MUCs from STM32H7, STM32F7 & STM32F4 which has same IC package - UFBGA176+25 (10 x 10 mm).

Any one MCU will be used in the design. Our intent is to change MCU based on needed performance without changing PCB layout design (i.e., drop-in replacement).

(1) STM32F429IIH6 (2) STM32F765IIK6 (3) STM32H743IIK6

Questions:

1) STM32F429IIH6, STM32F765IIK6 and STM32H743IIK6 are direct drop-in replacements?

2) Comparison chart attached for these 3 MCUs. Is there any reason why H743 is lesser cost as compared to other F765 & F429?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0