2025-08-11 12:28 AM
hello everyone ,
As i am trying to create a PCB project for my university project with stm32 MCU , at the moment i am kind of stuck in process of finding optimal filter circuit one needs to implement for optimal functioning , i have been reading through all the materials i can find and least to say there are many mixed suggestion and i also watched the stm webminar and MOOC for USB but i am even more confused,
so if any one can give me link for a working project or just material that can help me implement my targetted components , any project that have implemented the suggested circuit will help
I am using M24M01 EEPROM , i want to add a USB-A port so that i can export saved files to USB thumbdrives and also add max232 module for serial communication
2025-08-12 2:54 AM
Hi @eva1000
For USB type A implementation you can follow the schematics provided here
common-mode EMI filter and ESD protection are essential for robust connection and clean signals. For reference MB1939.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-08-12 3:04 AM
Check out ST's Application Notes; eg,
AN4879: Introduction to USB hardware and PCB guidelines using STM32 MCUs
@eva1000 wrote:i am trying to create a PCB project for my university project with stm32 MCU
What STM32, exactly?
For each family, you should find a Hardware Development guide; eg,
AN2586: Getting started with STM32F10xxx hardware development.
As @FBL suggested, check-out the schematics for ST's boards.
@eva1000 wrote:add max232 module for serial communication
Is this a retro design project?!
2025-08-12 8:15 AM
@eva1000 wrote:max232 module for serial communication
The MAX232 is a 5V part - so not suitable for use with STM32.
Plenty of 3V alternatives are available ...