2025-12-18 2:24 AM - last edited on 2025-12-18 3:57 AM by Andrew Neil
Hello,
We need to add WiFi connectivity to an STM32N6570-DK board and run Zephyr on it.
Is that possible? Can you propose a solution?
We have seen X-NUCLEO-67W61M1 expansion board that can work with STM32N6. But can that board be connected with the DK board?
Thank you very much for any suggestion.
Regards.
2025-12-18 2:34 AM
Of course it can - just connect appropriate pins for SPI, UART, GPIO ...
You will have to check the User Guides and/or schematics of both boards to find appropriate available pins.
2025-12-18 3:41 AM
Thank you for the quick response.
What about the software side? Any clue what would be needed to run zephyr?
Thanks
2025-12-18 3:56 AM
@mtv wrote:Any clue what would be needed to run zephyr?
You'd need to go to the Zephyr site for that:
https://docs.zephyrproject.org/latest/boards/st/stm32n6570_dk/doc/index.html
https://docs.zephyrproject.org/latest/samples/net/wifi/README.html
Getting started on Zephyr is a non-trivial journey:
2025-12-18 4:44 AM
However, with some effort it is possible, correct?
Otherwise a FreeRTOS implementation is more easy to implement using X-CUBE-ST67W61.
Have I understood it correctly?