2025-02-06 08:47 AM
Hi,
STM32N6570-DK preloaded code works with the default MB1854B camera board. My question is:
"Does the default firmware support VD66GY?"
I tried and could not make it work.
When I switch the camera module to VD66GY S-BOARD, the LCD shows "Camera not detected, power off board, connect camera, power on board". I double checked my S-BOARD with STEVAL-EVK-U0I (PCB4405C) and it works fine. I also checked the FFC connection to make sure the TYPE B cable has to be used for my S-BOARD instead of TYPE A cable included in the DK kit.
Thanks,
Jimmy