2025-01-05 9:20 AM - last edited on 2025-03-24 1:41 AM by Amel NASRI
Hi! I am new in electronics, but I am trying to design my PCB using STM32F469IIT6. I did a similar project before using a simple atmega168, but the STM32 seems way more complex. I wonder what the minimum of hardware connection is I need to be able to BOOT or even detect the target using my ST-LINK. Right now, I powered all VDD pins and VDDA pins, as well connected all the GND pins. I set up pins 137-SWCLK and 128-SWDIO in my IDE, connected the ST-LINK, but it does not find the target. I wish someone could give me a help.
Thank you!
Solved! Go to Solution.
2025-01-05 10:09 AM
@LucasStartTech And please don't try any of these ST-Links in colourful tin cans, because they are all fakes and don’t get recognized by the STM32CubeIDE. Instead, use an original ST-Link from a trustworthy retailer (i.e. not Alibaba or similar) so that the connection can be established.
Good luck!
/Peter
2025-01-05 9:46 AM
Dear @LucasStartTech ,
Welcome in our Community , Herr is a link for the minimum hardware setup required for STM32F4 series : https://www.st.com/resource/en/application_note/an4488-getting-started-with-stm32f4xxxx-mcu-hardware-development-stmicroelectronics.pdf
And below for F469 MCU :
To better help , if you can provide schematics around all power and dedicated pins in particular PDR_On, Bypass_Reg and VCAPxx pins .
let us know ,
Cheers,
STOne-32
2025-01-05 10:09 AM
@LucasStartTech And please don't try any of these ST-Links in colourful tin cans, because they are all fakes and don’t get recognized by the STM32CubeIDE. Instead, use an original ST-Link from a trustworthy retailer (i.e. not Alibaba or similar) so that the connection can be established.
Good luck!
/Peter
2025-01-05 10:41 AM
Check part orientation
Check voltage present on VCAP pin, and capacitors
Check voltage observed on NRST pin
Provide a schematic, constrained to the STM32 if that's simpler, so we can better understand what you've built.
A large, clear and in-focus picture of the board with the part in-situ will also be illustrative.
The ST-LINK expects to see a target voltage on pin 1 or 2 of the standard JTAG 20-pin connector.
2025-01-06 10:55 AM
Hi! I've been following the diagrams, they really help! I bought an adapter, where I then soldered the MCU to be able to kind of work in the breadboard. I wired the pins in the diagram, but the ST-link did not find the target. I also got another ST-LINK as Peter suggested, and I thinking in manufacture one version, for I am wondering if the distance of the capacitors from the VDD pins are one of the reasons for my constant failure. I will post the schematic I have so far. Thank you very much!
2025-01-06 10:56 AM
Thank you, Peter! I got both ST-LINKS, but I've only tried the cheap one. I will port the schematic and also, I will try the other ST-LINK.
Thank you!!
2025-01-06 9:06 PM
I was working on it today, and that's what I have so far... This the first PCB I have ever designed, so I appologize for any *** wiring. Thank you again!
2025-01-07 3:40 PM
Thread then went here https://community.st.com/t5/stm32-mcus-products/booting-stm32f469/td-p/759281
Sounds like an orientation issue