2019-02-18 1:26 AM
I am trying to read nfc cards with X-NUCLEO-NFC03A1 plugged on top of NUCLEO-L476RG. However, in the X-CUBE-NFC3 ver. 1.4.0 there is no example for such combination, but according to UM2045 Rev 2 ("The software comes with examples of implementation of such drivers, running on X-NUCLEO-NFC03A1 plugged on top of one NUCLEO-L476RG, NUCLEO-F401RE or NUCLEO-F103RB. ") somewhere should be such an example.
Could you please point out exactly where this example project can be downloaded?
Thanks in advance!
Linards
Solved! Go to Solution.
2019-02-18 5:20 AM
Hi @LGrig ,
Yes you are right, the documentation is indicating the L4 platform, but it is not present in the software package, this is a mistake. Please have a look to the following thread https://community.st.com/s/question/0D50X00009sUl5WSAS/read-the-rfid-of-a-card-with-nfc03a1, I've already made the porting to this platform for someone.
Let me know if that helps you.
Regards.
2019-02-18 5:20 AM
Hi @LGrig ,
Yes you are right, the documentation is indicating the L4 platform, but it is not present in the software package, this is a mistake. Please have a look to the following thread https://community.st.com/s/question/0D50X00009sUl5WSAS/read-the-rfid-of-a-card-with-nfc03a1, I've already made the porting to this platform for someone.
Let me know if that helps you.
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.