2021-10-19 4:38 AM
I have BL654 as a tag. When reading it from the ST-25 Android app it receives 992 as mentioned below. Whereas the write data size in the tag is only 14 bytes. Can you please explain this behavior?
-- Data receive on ST-25 Android App ---------
NFC type 2 Tag
CCLEN:4
Magic Number 0xE1
Mapping Version 10
Memory size of 992 bytes
Read Access 0
Write Access F
--------------------------------------------------------
Thank You,
Bhavin.
Solved! Go to Solution.
2021-10-20 12:44 AM
Hi Bhavin,
I can help to clarify a few things:
Best regards
Olivier
2021-10-19 4:49 AM
Hi
992 corresponds to the size of the T2T_Area, it comes from the byte CC2 of the CCFile (read Block 3). This tag is not from STMicroelectronics so I'm not able to tell you more.
The 14 bytes that you mention are probably the 14 bytes of the NDEF file contained in this tag, isn't it?
I can see from the Write Access that this tag is Read Only so it is not possible to write it.
Regards
Olivier
2021-10-19 10:22 PM
HI Olivier,
Here is a link for data format of Nordic BL654. Please help me to identify Why it's send's 992 bytes. As per link i found that TVL blocks contain up to a maximum data size as 992 bytes. But I can not relate it because we only write 14 bytes. Once more thing is that on nordic mobile app it's read only 14 bytes (Please look at link).
As per my limited knowledge in NDEF : I am understanding that all the tag reading software should follow same logic for read NDEF message irrespective of it's manufacturer, So why Nordic and ST25 mobile app work differently.
Thank You,
Bhavin
2021-10-20 12:44 AM
Hi Bhavin,
I can help to clarify a few things:
Best regards
Olivier
2021-10-20 1:09 AM
Hi Oliver,
Please let me know if you need more information.
Thank you,
Bhavin.
2021-10-20 1:16 AM
Hi,
The values that I gave are examples. I don't know if this tag has 1024 bytes of memory. i used this example to explaine the difference between the total memory, the T2T_Area size and the NDEF TLV size.
I can't tell you more about this tag that is not an STMicroelectronics tag. You might be interested by our ST25TN tag which is also an NFC Type 2 tag: https://www.st.com/en/nfc/st25tn-series-nfc-tags.html
Regards
Olivier
2021-10-20 1:52 AM
Hi Olivier,
We have to give support to third party tag in already released product it's not in our control.
During this i also have test with STM library and found something use full.
Please look at link.
At line no 163: buffer[16] have 124. So total size become 992 Bytes that's exactly match with ST25 app data.
i have following query based on this findings.
Thank You,
Bhavin.
2021-10-20 2:02 AM
Hi Bhavin,
As per NFC Forum Type 2 spec, CC File location is in block 3. CC2 is the third byte of this CCFile block. This is the byte 14 if you look from the beginning of memory.
CC2 contains encoding for the size of the T2T_Area. The actual size of the T2T_Area (in bytes) is calculated with the formula: T2T_Area_Size = Size*8.
We indeed have T2T_Area_size = 124 * 8 = 992.
CC2 value (equal to 124) is received directly from the tag.
Regards
Olivier
2021-10-20 2:16 AM
HI Olivier,
Is this CC2 value (124 Byte) it's Fixed for all the case? ( if not please describe how it's value change based on tag writing method in context of NDEF standard )
Thank you,
Bhavin
2021-10-20 2:22 AM
It depends of the tag. I suggest that you contact the manufacturer of this tag to ask them if CC2 can be changed or not for this tag.
If it is not locked in read only mode, you can write it by writing an ordinary block.
Best regards
Olivier