cancel
Showing results for 
Search instead for 
Did you mean: 

What reading performance (tags/seconds) can be achieved with the ST25RU3993 and what are the best reader settings for a high reading rate?

Raphael_Ko
Associate II
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Bart Herse
Senior II

Hi User15749752844702162942,

the maximum sustained read rate that can be achieved with the ST25RU3993 for 96 bit tag EPC length is by using a backscatter link frequency (BLF) of 640 kHz.

  • M2 coding --> 600 tag reads/sec
  • FM0 coding --> 760 tag reads/sec

The maximum read rate that can be used at full power depends on the country/region and their respective radio regulation laws.

Accounting for a dense reader environment also puts restrictions on the maximum read rate (see channel boundary backscatter).

Cheers,

B

View solution in original post

1 REPLY 1
Bart Herse
Senior II

Hi User15749752844702162942,

the maximum sustained read rate that can be achieved with the ST25RU3993 for 96 bit tag EPC length is by using a backscatter link frequency (BLF) of 640 kHz.

  • M2 coding --> 600 tag reads/sec
  • FM0 coding --> 760 tag reads/sec

The maximum read rate that can be used at full power depends on the country/region and their respective radio regulation laws.

Accounting for a dense reader environment also puts restrictions on the maximum read rate (see channel boundary backscatter).

Cheers,

B